Good things come in small packages?
A lot has been done to provide greater capacitance in smaller packages for ceramic and electrolytic capacitors, for use in bypass applications. It is worth noting that electrolytic and ceramic capacitors exhibit appreciable dielectric absorption, or DA. This is a non-linear behavior causing the capacitor to have a large time-dependent charge or discharge factor, when a voltage or short is applied. It is usually modeled as a number of different value series R-C pairs connected in parallel with the main capacitor. This causes the capacitor to take considerable time to reach its final steady state near-zero current when a voltage is applied or changed. When trying to test the true leakage current on a DUT it may be necessary to wait until the current on any bypass capacitors has reached steady state before a current measurement is taken. Depending on the test time and capacitor being used this could result in an unacceptably long wait time.
So how do they compare?
In Figure 1 I captured the time-dependent current response waveform for a 5.1 megohm resistor, a 5.1 megohm resistor in parallel with 100 microfarad electrolytic capacitor, and finally a 5.1 megohm resistor in parallel with 100 microfarad film capacitor, when a 5 volt step stimulus was applied.

The 5.1 megohm resistor (i.e. “no capacitor”) serves as a base line to compare the affect the two different bypass capacitors have on leakage current measurement. The film capacitor has relatively ideal electrical characteristics in comparison to an equivalent electrolytic or ceramic capacitor. It settles down to near steady state conditions within 0.5 to 1 second. At 3 to 3.5 seconds out (marker placement in Figure 1) the film capacitor is contributing a fairly negligible 42 nanoamps of additional leakage. In comparison the electrolytic capacitor current is still four times as great as the resistor current and nowhere near being settled out. If you ever wondered why audio equipment producers insist on high performance film capacitors in critical applications, DA is one of those reasons!
So how long did it take for the electrolytic capacitor to reach steady state? I set up a longer term capture in Figure 2 for the electrolytic capacitor. After about a whopping 40 seconds later it seemed to be fully settled out, but still contributing a substantial 893 nanoamps of additional steady state leakage current.

Where do I go from here?
So what should one do when needing to test leakage current? When testing a wireless device be aware of what kind and value of bypass capacitor has been incorporated into it. Most likely it is a ceramic capacitor nowadays. Film capacitors are too large and cost prohibitive here. Find out how long it takes to settle to its steady state value. Also, off-state current measurements are generally left until the end of the testing to not waste time waiting for the capacitor to reach steady state. If testing a component, if a bypass capacitor is being used on the test fixture, consider using a film capacitor. With test times of just seconds and microamp level leakage currents the wrong bypass capacitor can be a huge problem!
No comments:
Post a Comment
Note: Only a member of this blog may post a comment.