tag:blogger.com,1999:blog-6161778274523938171.post1126634254488785713..comments2023-06-23T04:41:12.261-04:00Comments on Watt's Up?: Why do I measure voltage to earth ground on a power supply with a floating output?GaryRhttp://www.blogger.com/profile/13342106993487479289noreply@blogger.comBlogger4125tag:blogger.com,1999:blog-6161778274523938171.post-62887417398438301832018-10-20T11:16:02.625-04:002018-10-20T11:16:02.625-04:00sir, i have doubt yestday i measured one dc charge...sir, i have doubt yestday i measured one dc charger o/p positive to ground = 52 V and negative to ground = 69 V total o/p voltage was 121 VDC, why it was not equal like 60.5 and 60.5<br />Ohmhttps://www.blogger.com/profile/02613454842884287755noreply@blogger.comtag:blogger.com,1999:blog-6161778274523938171.post-75864274443746905802018-08-26T08:33:27.148-04:002018-08-26T08:33:27.148-04:00how can i detect the supply voltage leakage to gro...how can i detect the supply voltage leakage to ground<br />Anonymoushttps://www.blogger.com/profile/17228792427950950141noreply@blogger.comtag:blogger.com,1999:blog-6161778274523938171.post-18740298516850261592016-03-21T13:23:56.896-04:002016-03-21T13:23:56.896-04:00This is a basic application of nodal analysis usin...This is a basic application of nodal analysis using Kirchhoff's Voltage Law. 511 K in parallel with 10 M yields 486.2 K. 486.2 K in series with the other 511 K yields 997.2 K. 20 V across 997.2 K yields a current of ~20 uA. 20 uA through the parallel combination of 486.2 K yields 9.7 V.GaryRhttps://www.blogger.com/profile/13342106993487479289noreply@blogger.comtag:blogger.com,1999:blog-6161778274523938171.post-45055524733398317172016-03-20T11:20:14.576-04:002016-03-20T11:20:14.576-04:00I don't understand how 9.7V Came kindly explai...I don't understand how 9.7V Came kindly explain it.NAILESHnoreply@blogger.com