Today’s system DC power supplies incorporate quite a variety of features to protect both the device under test (DUT) as well as the power supply itself from damage due to a fault condition or setting mishap. Over voltage protect (OVP) and over current protect (OCP) are two core protection features that are found on most all system DC power supplies to help protect against power-related damage.
OVP helps assure the DUT is protected against power-related damage in the event voltage rises above an acceptable range of operation. As over voltage damage is almost instantaneous the OVP level is set at reasonable margin below this level to be effective, yet is suitably higher than maximum expected DUT operating voltage so that any transient voltages do not cause false tripping. Causes of OV conditions are often external to the DUT.
OCP helps assure the DUT is protected against power-related damage in the event it fails in some fashion causing excess current, such as an internal short or some other type of failure. The DUT can also draw excess current from consuming excess power due to overloading or internal problem causing inefficient operation and excessive internal power dissipation.
OVP and OCP are depicted in Figure 1 below for an example DUT that operates at a set voltage level of 48V, within a few percent, and uses about 450W of power. In this case the OVP and OCP levels are set at about 10% higher to safeguard the DUT.
Figure 1: OVP and OCP settings to safeguard an example DUT
However, not all DUTs operate over as limited a range as depicted in Figure 1. Consider for example many, if not most all DC to DC converters operate over a wide range of voltage while using relatively constant power. Similarly many devices incorporate DC to DC converters to give them an extended range of input voltage operation. To illustrate with an example, consider a DC to DC converter that operates from 24 to 48 volts and runs at 225W is shown in Figure 2. DC to DC converters operate very efficiency so they dissipate a small amount of power and the rest is transferred to the load. If there is a problem with the DC to DC converter causing it to run inefficiently it could be quickly damaged due to overheating. While the fixed OCP level depicted here will also adequately protect it for over power at 24 volts, as can be seen it does not work well to protect the DUT for over power at higher voltage levels.
Figure 2: Example DC to DC converter input V and I operating range
A preferable alternative would instead be to have an over power protection limit, as depicted in Figure 3. This would provide an adequate safeguard regardless of input voltage setting.
Figure 3: Example DC to DC converter input V and I operating range with over power protect
As an over power level setting is not a feature that is commonly found in system DC power supplies, this would then mean having to change the OCP level for each voltage setting change, which may not be convenient or desirable, or in some cases practical to do. However, in the Agilent N6900A and N7900A Advance Power System DC power supplies it is possible to continually sense the output power level in the configurable smart triggering system. This can in turn be used to create a logical expression to use the output power level to trigger an output protect shutdown. This is depicted in Figure 4, using the N7906A software utility to graphically configure this logical expression and then download it into the Advance Power System DC power supply. As the smart triggering system operates at hardware speeds within the instrument it is fast-responding, an important consideration for implementing protection mechanisms.
Figure 4: N7906A Software utility graphically configuring an over power protect shutdown
A glitch delay was also added to prevent false triggers due to temporary peaks of power being drawn by the DUT during transient events. While the output power level is being used here to trigger a fault shutdown it could have been just as easily used to trigger a variety of other actions as well.
Showing posts with label DC/DC converter. Show all posts
Showing posts with label DC/DC converter. Show all posts
Monday, June 23, 2014
Safeguarding your power-sensitive DUTs from an over power condition
Labels:
Advanced Power System,
APS,
constant power,
DC/DC converter,
fault protection,
N6900,
N7900,
N7906A,
over power,
over power protect,
over voltage protect,
over-current protection,
OVP,
Usage
Wednesday, May 14, 2014
European Space Power Conference (ESPC) for 2014
This week’s blog posting is going in a bit of a different
direction, as I likewise did last month, to attend and participate in the 2014 European
Space Power Conference (ESPC) for 2014. While this was the tenth ESPC, which I
understand takes place every couple of years; this was the first time I had
opportunity to attend. One thing for certain; this was all about DC power,
which is directly aligned with the things I am always involved in. In this particular
instance it was all about DC power for satellites and space-bound crafts and
probes.
I initially found it just a bit curious that a number of
the keynote speeches also focused a fair amount on terrestrial solar power as
well, but I supposed I should not be at all surprised. There has been a large
amount of innovation and a variety of things that benefit our daily lives that
came out of our own space program, fueled by our involvement in the “space
race” and still continuing on to this day. (Can you name a few by chance?).
This is a natural progression for a vast number of technological advances we
enjoy.
At ESPC there were numerous papers presented on solar
cells and arrays, batteries and energy storage, nuclear power sources, power
conversion and DC/DC converters, super-capacitors, and a variety of other
topics related to power. Just a couple of my learnings and observations
include:
·
There was a very high level of collaboration of
sharing findings and answering questions among peers attending the event
·
While batteries generally have very limited
lives, from findings presented, it was interesting to see how well they have
performed over extended periods in space, lasting last well in excess of their
planned life expectancies. It is a reflection of a combination of several
things including careful control and workmanship, understanding life-shortening
and failure mechanisms, how to take properly treat them over time, what should
be expected, as well as other factors contributing to their longevity. I expect
this kind of work will ultimately find its way to being applied to using
lithium ion batteries in automotive as well.
·
A lot of innovation likewise continues with
solar cell development with higher conversion efficiencies coming from
multi-junction devices. Maybe we’ll see this become commonplace for terrestrial
applications before long!
·
A number of research papers were presented from
participants from universities as well. In all, the quality of work was
excellent.
I was there with another colleague, Carlo Canziani. Together
we represented some of our DC power solutions there, including our N7905A DC
Power Analyzer, N7900 series Advanced Power System (APS), and E4360A series Solar
Array Simulator (SAS) mainframe and modules. These are the kinds of advanced
power stimulus and measurement test instruments vital for conducting testing on
satellite and spacecraft power components and systems.
Labels:
Advanced Power System,
DC Power Analyzer,
DC/DC converter,
ESPC,
European Space Power Conference,
Misc.,
N6705B DC Power Analyzer,
N7900,
SAS,
solar array simulator,
solar cell test
Monday, February 24, 2014
How to test the efficiency of DC to DC converters, part 2 of 2
In part 1 of my posting on testing the efficiency of DC
to DC converters (click here to review) I went over the test set up, the
requirements for load sweep synchronized to the measurements, and details of
the choice of the type and set up of the current load sweep itself. In this
second part I will be describing details of the measurement set up, setting up the
efficiency calculation, and results of the testing. This is based on using the
N6705B DC Power Analyzer, N6782A SMUs, and 14585A software as a platform but a
number of ideas can be applicable regardless of the platform.
Figure 1: Synchronized measurement and efficiency
calculation set up
The synchronized measurement and efficiency calculation
set up, and display of results are shown in Figure 1, taking note of the
following details corresponding to the numbers in Figure 1:
- In the 14585A the data logging mode was selected to make and display the measurements. The oscilloscope mode could have just as easily been used but with a 10 second sweep the extra speed of sampling with the oscilloscope mode was not an advantage. A second thing about using the data logging mode is you can set the integration time period for each acquisition point. This can be used to advantage in averaging out noise and disturbances as needed for a smoother and more representative result. In this case an integration period of 50 milliseconds was used.
- To synchronize the measurements the data log measurement was set to trigger off the start of the load current sweep.
- Voltage, current, and power for both the input and output SMUs were selected to be measured and displayed. The input and output power are needed for the efficiency calculation.
- The measurements were set to seamless ranging. In this way the appropriate measurement range for at any given point was used as the loading swept from zero to full load.
- A formula trace was created to calculate and display the efficiency in %. Note that the negative of the ratio of output power to input power was used. This is because the SMU acting as a load is sinking current and so both its current and power readings are negative.
With all of this completed really all that is left to do
is first start the data logging measurement with the start button. It will be
“armed” and waiting from a trigger signal from the current load sweep ARB that
had been set up. All that is now left to do is press the ARB start button.
Figure 2 is a display of all the results after the sweep is completed.
Figure 2: DC to DC Converter efficiency test results
All the input and output voltage, current, and power
measurements, and efficiency calculation (in pink) are display, but it can be
uncluttered a bit by turning off the voltages and currents traces being
displayed and just leave the power and efficiency traces displayed. This
happened to be special DC to DC converter designed to give exceptionally high
efficiency even down to near zero load, which can be seen from the graph. It’s
interesting to note peak efficiency occurred at around 60% of full load and
then ohmic losses start becoming more significant.
Labels:
CC mode,
constant current,
DC electronic load,
DC Power Analyzer,
DC/DC converter,
digitizer,
electronic load,
ELOG. datalog,
N6705B DC Power Analyzer,
N6782A,
power efficiency,
Usage
Thursday, February 20, 2014
How to test the efficiency of DC to DC converters, part 1 of 2
I periodically get asked to provide recommendations and
guidance on testing the efficiency of small DC to DC voltage converters. Regardless
of the size of the converter, a DC source is needed to provide input power to
the converter under constant voltage, while an electronic load is needed to
draw power from the output, usually under constant current loading. The load
current needs to be swept from zero to the full load current capability of the
DC to DC converter while input power (input voltage times input current) and
output power (output voltage times output current) are recorded. The efficiency
is then the ratio of power out to power in, most often expressed in a
percentage. An illustration of this is shown in Figure 1. In addition to sourcing
and sinking power, precision current and voltage measurement on both the input
and output, synchronized to the sweeping of the load current is needed.
Figure 1: DC to DC converter efficiency test set up
One challenge for small DC to DC voltage converters is
finding a suitable electronic load that will operate at the low output voltages
and down to zero load currents, needed for testing their efficiency over their
range, from no load to full load output power. It turns out in practice many
source measure units (SMUs) will serve well as a DC electronic load for
testing, as they will sink current as well as source current.
Perhaps the most optimum choice from us is to use two of
our N6782A 2-quadrant SMU modules installed in our N6705B DC Power Analyzer
mainframe, using the 14585A software to control the set up and display the
results. This is a rather flexible
platform intended for a variety of whatever application one can come up with
for the most part. With a little ingenuity it can be quickly configured to
perform an efficiency test of small DC to DC converters, swept from no load to
full load operation. This is good for converters of 20 watts of power or less
and within a certain range of voltage, as the N6782A can source or sink up to 6
V and 3 A or 20 V and 1 A, depending on which range it is set to. One of the
N6782A operates as a DC voltage source to power the DUT and the second is
operated as a DC current load to draw power from the DUT. A nice thing about
the N6782A is it provides excellent performance operated either as a DC source
or load, and operated either in constant voltage or constant current.
An excellent video of this set up testing a DC to DC
converter was created by a colleague here, which you can review by clicking on
the following link: “DC to DC converter efficiency test”.
The video does an excellent job covering a lot of the
details. However, if you are interested in testing DC to DC converters using
this set up I have a few more details to share here about it which should help
you further along with setting it up and running it.
First, the two N6782A SMUs were set up for initial operating
conditions. The N6782A providing DC power in was set up as a voltage source at
the desired input voltage level and the second N6782A was set to constant
current load operation with minimum (near zero) loading current.
Note that the 14585A software does not directly sweep the
load current along the horizontal axis. The horizontal axis is time. That is
why a time-based current sweep was created in the arbitrary waveform (ARB) section
of the 14585A. In that way any point on the horizontal time axis correlates to
a certain current load level being drawn from the output of the DUT. The ARB of
course was set to run once, not repetitively. The 14585A ARB set up is shown in
Figure 2.
Figure 2: Load current sweep ARB set up in 14585A
software
This ARB sweep requires a little explanation. While there are a number of pre-defined ARBs,
and they can be used, an x3 power formula was chosen to be used
instead. This provided a gradually increasing load sweep that allowed greater
resolution of this data and display at light loads, where efficiency more
quickly changes. As can be seen, the duration of the sweep, parameter x, was
set to 10 seconds. As a full load current needed to be -1 A, using the actual formula
(-x/10)3 gave us a gradually
increasing load current sweep that topped out at -1A after 10 seconds of
duration. The choice of 10 seconds was arbitrary. It only provided an easy way
to watch the sweep on the 14585A graphing as it progressed. Finally, a short
(0.1 second) pre-defined linear ramp ARB was added as a second part of the ARB
sequence, to bring the load current back to initial, near zero, load conditions
after the sweep was completed. This is shown in Figure 3.
Figure 3: Second part of ARB sweep to bring DUT load
current back to initial conditions
I hope this gives you a number of insights about creative
ways you can make use of the ARB. As there is a good amount of subtle details on
how to go about making and displaying the measurements I’ll be sharing that in
a second part coming up shortly, so keep on the outlook!
Labels:
CC mode,
CV mode,
DC electronic load,
DC Power Supply,
DC/DC converter,
electronic load,
N6705B DC Power Analyzer,
N6782A,
power efficiency,
SMU,
Usage
Monday, October 15, 2012
Flyback Inverter for Fluorescent Lamp: Part 2, A Little Theory of Operation
In part 1 of this posting “Flyback Inverter for
Fluorescent Lamp: Part 1, Making Repairs” a little careful and straightforward
troubleshooting and repair brought my friend’s fluorescent lamp assembly back
to life again. But a fluorescent lamp has quite a few unique requirements to
get it to start up and stay illuminated. How does this flyback converter manage
to do these things?
I had first looked around to see if I could find a
schematic for this fluorescent lamp assembly, but nothing turned up for me.
However, the parts count was low enough, and circuit board large enough, that
it was a fairly simple matter to trace out and sketch the inverter’s schematic
in fairly short order, as shown in Figure 1.
Figure 1: Fluorescent lamp single-ended flyback inverter
circuit
When first powered up the switching transistor is biased
on by the 812 ohm resistor, energizing transformer winding W1. This in turn
applies positive feedback to the transistor through winding W2, driving it into
saturation. There are two mechanisms in the flyback transformer that are
critical for making this inverter work:
- First it has a gapped core. This allows it to store a substantial amount of energy in its magnetic field which in turn gets dumped over to the fluorescent tube through the secondary winding W3 when the transistor turns off and the transformer’s magnetic field collapses. During this period the winding voltage continues to climb as the magnetic field collapses until the energy can find a place to discharge to, in this case into the fluorescent tube. The voltage is also further increased by the turns ratio of the transformer. This is the “flyback” effect that creates sufficiently high enough voltage to get the fluorescent tube to “strike” or ionize its gas to get it to start conducting and give off illumination, typically many hundreds of volts.
- As can be seen this inverter is a very simple circuit with a minimum of parts. A second mechanism in the transformer is it is designed to saturate in order to make the inverter oscillate. At the end of the transistor’s “on” period the transformer reaches its maximum magnetic flux at which point the transformer saturates. Winding voltage W2 drops to zero and then reverses driving the switching transistor into cutoff. After the magnetic field has collapsed and energy discharged to the fluorescent tube the process repeats itself.
The switching transistor’s collector and base voltages
during turn on are captured in the oscilloscope diagram shown in Figure 2.
Figure 2: Inverter switching transistor collector and
base voltage waveforms
A number of interesting things can be observed in Figure
2. The oscillation period is roughly 50
microseconds, or oscillation frequency of 20 kHz. It takes about 10 cycles, 500
microseconds, for the fluorescent tube to strike. During this initial phase the
peak collector voltage is flying up to nearly 100 volts or about 8 times the DC
input voltage being applied. Again, this voltage is being multiplied up by the
turns ratio of windings W1 and W2 to bring this up in the vicinity of 600 volts
or so needed to make the fluorescent tube to strike. Once the tube does strike
and starts conducting its impedance drops. This causes the collector voltage to
drop down to about 35 volts which is consistent with the proportion of drop in
voltage needed for the fluorescent tube once it’s gas is ionized and is
conducting. Note also the collector voltage pulse also widens as it takes a
longer time for the energy in the transformer to be dumped when it’s at a lower
voltage.
Although this inverter at first glance is a rather simple
and minimum viable, minimum parts count circuit, with careful design it can be
made to be very efficient. This is where the design of the transformer becomes
as much art as science, knowing how the subtle characteristics of the magnetic
material and inductive and capacitive parasitics can be used to advantage in
contributing to and improving the overall performance of the design.
Anyway, what my friend really cared about is the lamp now
works and he is able to put it to good use in his camper!
Wednesday, May 16, 2012
What Is Old is New Again: Soft-Switching and Synchronous Rectification in Vintage Automobile Radios
I have to admit I am a bit of a vintage electronics
technologist. One of many pass times
includes bringing vintage vacuum tube automobile radios back to life. In
working with modern DC sources I’ve seen innovations come about in the past
decade for efficient power conversion, including soft switching and synchronous
rectification. A funny thing however, for those who have been around long
enough, or into vintage technologies like me, is that these issues and somewhat
comparable solutions existed up to 70 years ago for automobile radios and other
related electronic equipment. What is old is new again!
As we know, vacuum tubes (or valves to many) were to
electronics back then as what semiconductors are to electronics today. The
problem for portable and mobile equipment was that the vacuum tubes needed
typically 100 or more volts DC to operate. They did have high voltage batteries
for portable equipment but for automobiles the radio really needed to run off
the 6 or 12 volts DC available from the electrical system. The solution: A
DC/DC boost converter!
Up until the mid 1950’s most all automobile radios used vacuum
tubes biased with high voltage generated from a rather primitive but clever
DC/DC boost converter design. The inherent technological challenge was
semiconductors did not yet exist to chop up the low-voltage, high-current DC to
convert it to high-voltage, low-current DC. Of course if the semiconductors did
exist this would all be a moot point! Making use of what was available the
DC/DC boost converters employed what were called vibrators, which are a form of
a continuously buzzing relay, to chop up the low-voltage DC for conversion.
Maybe some of you are familiar with the soft humming sound heard when an
original vintage automobile radio is turned on, prior to the vacuum tubes
finally warming up and the audio taking over? That humming is the vibrator, the
“heart” of the DC/DC boost converter in the radio.
Figure 1 below is an example circuit of vibrator-based
DC/DC boost converter in a vintage automobile radio. This is just one of quite
variety of different implementations created back then. Two pairs of contacts in
the vibrator act in a push-pull fashion to convert the low-voltage DC into a
low-voltage AC square wave. This in turn is converted to a high-voltage square
wave by the transformer. Because the vibrator is an electro-mechanical device,
it is limited in how fast it can switch. Switching frequencies are typically
about 100 to 120 Hz. The transformers used are naturally the steel-laminated
affairs similar in nature to the transformers used to convert household line
voltage in home appliances. Very possibly some radio manufacturers used off-
the-shelf appliance transformers in reverse to step up the voltage! Often a small rectifier vacuum tube, such as a
6X4 (relatively modern, by vacuum tube standards) would be used to convert the
high voltage AC to high voltage DC, but in this particular example I am showing
here another two pairs of contacts on the secondary side switch simultaneously
with the first pairs of contacts to rectify the high voltage AC. Highly
efficient synchronous rectification, up to 70 years ago!
The clever part of these DC/DC boost converters is making
the vibrators last. Let’s see; 100 cycles/second, times 60 seconds/minute,
times 60 minutes/hour, times ~2 hours/day, times 365 days/year; that’s 263 million cycles in one year! And while
the vibrator was replaceable, it would often last for many years or more, which
is quite remarkable. The trick was paying close attention to the switching as
to not stress the vibrator‘s contacts. Referring to the waveforms in Figure 2,
there is quite a bit of dead time between the non-overlapping switching of the
contacts. This was by design. The capacitor across the secondary of the
transformer in Figure 1 is carefully matched to ring with the transformer’s
inductance such that the voltage is near zero across the alternate set of
contacts is just as they’re closing, minimizing arcing and wear. Low-stress
soft switching, again, up to 70 years ago! Ironically the cause for the
vibrator failing was often due the capacitor degrading with stress and time. The
capacitor was actually slightly larger than ideal value at the start to prevent
overshoot and allow for aging. When resurrecting a vintage automobile radio frequently
the vibrator will still work. Make certain to replace the capacitor first
however or the vibrator is bound to have a very short second life.
These vacuum tube automobile radios with vibrator-based
DC/DC boost converters had quite a long run before being displaced, first for a
very short period in the later 1950’s by hybrid radios using low voltage vacuum
tubes and early germanium power transistors, and then finally overtaken by
fully transistorized automobile radios in the early 1960’s.
So my hat’s off to the many design engineers of
yesteryear who encountered such challenges, fully understood the principles, and
just as creatively came up with solutions for them so long ago, based on what
they had available. And again for those seasoned engineers who see such things
come around yet once more as a new innovation, who humbly smile to themselves
knowing that “what is old is new again”.
By chance are you a vintage electronics technologist?
Labels:
DC/DC converter,
inverter,
Misc.,
power supply,
soft switching,
switching power supply,
synchronous rectification,
vacuum tube automobile radio,
vacuum tube radio,
valve radio,
vintage radio
Subscribe to:
Posts (Atom)