Eighteen months ago, in September of 2013, Keysight (we were Agilent at the time) introduced a new high-power series of power supplies: the N8900 series of 5 kW, 10 kW, and 15 kW autoranging DC power supplies. I posted about those here.
Recently, our environmental lab was doing some testing on one of the 15 kW models that required them to use a low-noise load on the output. They have electronic loads that they can connect to the output to dissipate this level of power, but to be sure they were getting the lowest noise possible, they wanted to use resistors to load the output instead of the electronic loads. Since I was amused by the size of the resistors, I thought I’d capture the moment and share a picture with you.
The picture shows one of our R&D engineers in our environmental lab adjusting the output voltage of a 15 kW N8900 series power supply. Notice that these power supplies pack a lot of power (15 kW) in their small 3 U high package (the white box under the fan). The four big green things on the rack are resistors. The two on the top rack are each rated for 15 kW while the two on the lower rack are each rated for 20 kW. So that’s a total of 70 kW of resistive power! Clearly, these are not your father’s ¼ W resistors!
Even with 70 kW of power dissipation capability, and “only” 15 kW available from our power supply, a big fan was needed to keep the resistors cool…..or perhaps I should say “less hot” since they still get very hot. Of course, with an extra 15 kW of power being dissipated in the room, the room temperature was going up. But that was a good thing since we are still experiencing cold weather here in New Jersey despite the fact that spring started ten days ago. So the extra heat felt good!
Before we came out with the N8900 series of high-power supplies, Matt had posted about some things around his desk that included a 2500 W resistor (click here for his post). At that time, that was a high-power resistor. But now with these 15 kW supplies, you can see we had to go much bigger! And given that these supplies can be paralleled to 100 kW or more….well….I look forward to seeing what our R&D group and environment lab engineers come up with to do resistive load testing on those. Submarine-sized resistors, perhaps? We’ll see….
Showing posts with label high power. Show all posts
Showing posts with label high power. Show all posts
Monday, March 30, 2015
Monday, November 24, 2014
Prewired rack delivers up to 90 kW of single-output DC power
As I have mentioned before, I avoid posting product-only-focused material in this blog since our goal is to educate about power-related items rather than to directly promote Keysight products. But when something new comes out, I like to announcement it here.
A little over a year ago, Keysight (we were Agilent at the time) announced a new power supply family with high-power outputs up to 15 kW per output (see link here). These high-power autoranging DC power supplies with individual outputs up to 1500 V or 510 A can be paralleled for even more power. Paralleling outputs with these supplies is simplified since multiple outputs can be grouped to act as a single output and the current share bus enables multiple outputs to more equally share current. But there are other considerations when paralleling multiple units. Wiring the AC inputs and DC outputs together takes design time and assembly time. Integrating the units together physically in a rack also takes time and effort. Designing the system to ensure the safety of operators is also very important. So Keysight decided to offer a prewired rack to help you overcome the challenges associated with racking high-power supplies.
On November 11, 2014 (less than 2 weeks ago), we announced a prewired rack that combines up to six of the 15 kW N8900 series power supplies for total power up to 90 kW from a single output. You can choose from a variety of DC output combinations with voltages from 80 V to 1500 V and currents from 60 A to 3060 A. That’s a lot of current! The rack’s internal configuration makes the multiple outputs appear as a single output allowing you to communicate with just one power supply through LAN, GPIB, or USB (all standard in the system). Click here for the press release for this new system and here for additional system information.
Perhaps you are working in R&D or manufacturing on EV/HEV, alternative energy (fuel cells, solar, etc.), industrial DC motors, large UPS’s, electroplating, or any of the many other high-power application areas that need DC power up to 90 kW with voltages to 1500 V or currents to 3060 A. If so, and you want to spend your engineering resources on your core competencies instead of racking power supplies together, let Keysight help you with our new N8900 Series Rack System.
A little over a year ago, Keysight (we were Agilent at the time) announced a new power supply family with high-power outputs up to 15 kW per output (see link here). These high-power autoranging DC power supplies with individual outputs up to 1500 V or 510 A can be paralleled for even more power. Paralleling outputs with these supplies is simplified since multiple outputs can be grouped to act as a single output and the current share bus enables multiple outputs to more equally share current. But there are other considerations when paralleling multiple units. Wiring the AC inputs and DC outputs together takes design time and assembly time. Integrating the units together physically in a rack also takes time and effort. Designing the system to ensure the safety of operators is also very important. So Keysight decided to offer a prewired rack to help you overcome the challenges associated with racking high-power supplies.
On November 11, 2014 (less than 2 weeks ago), we announced a prewired rack that combines up to six of the 15 kW N8900 series power supplies for total power up to 90 kW from a single output. You can choose from a variety of DC output combinations with voltages from 80 V to 1500 V and currents from 60 A to 3060 A. That’s a lot of current! The rack’s internal configuration makes the multiple outputs appear as a single output allowing you to communicate with just one power supply through LAN, GPIB, or USB (all standard in the system). Click here for the press release for this new system and here for additional system information.
Perhaps you are working in R&D or manufacturing on EV/HEV, alternative energy (fuel cells, solar, etc.), industrial DC motors, large UPS’s, electroplating, or any of the many other high-power application areas that need DC power up to 90 kW with voltages to 1500 V or currents to 3060 A. If so, and you want to spend your engineering resources on your core competencies instead of racking power supplies together, let Keysight help you with our new N8900 Series Rack System.
Labels:
90 kW,
high power,
high power rack,
Misc.,
N8900,
power supply,
power supply rack
Monday, September 30, 2013
New Agilent Advanced Power System: More on High-Power!
Last week, I announced two new families of high-power system
DC power supplies from Agilent Technologies:
- N6900/N7900 Series 1- and 2-kW Advanced Power System (APS) DC Power Supplies
- N8900 Series 5-, 10-, and 15-kW Autoranging DC Power Supplies
In my post last week, I concentrated on the N8900 Series of
autoranging power supplies. Those are basic DC power supplies with outputs up
to 15 kW (can be paralleled to 100 kW and more). Today, I am focusing on the
N6900/N7900 Series of Advanced Power System DC Power Supplies. These power
supplies really do live up to their “Advanced Power System” label. I’ve been
working here on power products since 1980 and have supported several feature-rich
product families in that time: most notable were our AC source products (6811B,
6812B, and 6813B) and more recently, our battery drain analysis source/measure
units (N6705B with N6781A). The new N6900/N7900 Advanced Power System rivals
those products for rich features and quite honestly, just like our marketing
slogan says, they really should help you “overcome your toughest power test
challenges”. Why? Read on…
First the basics:
- There are ten 1 kW models each in a 1U package
- There are fourteen 2 kW models each in a 2U package
- Rated output voltages range from 9 V to 160 V
- Rated output currents range from 12.5 A to 200 A
- Outputs can be paralleled up to 10 kW
Now for a few details. There are two performance levels:
- N6900 Series is designed for ATE applications where high performance is critical
- N7900 Series is designed for ATE applications where high-speed dynamic sourcing and measurement is needed
Sourcing
- Precision voltage and current programming (N6900 is 14-bit; N7900 is 16-bit)
- Programmable output resistance
- Current sinking up to 10% of rated current (up to 100% with added N7909A power dissipator)
- 18-bit voltage and current measurements
- Power measurements
- Amp-Hour and Watt-Hour measurements
The higher performance N7900 products add more features to the above:
Sourcing
- Precision 16-bit voltage and current programming (N6900 is 14-bit)
- Output lists to quickly step through voltage or current levels
- Arbitrary waveform generation
- Low current measurement range
- Seamless ranging for dynamic current measurements
- Adjustable sample rate
- Measurement array readback
- External data logging
And even more capabilities:
- Extended current measurement range that measures 2.25 x higher than the rated current
- Sampling up to 200 kS/s
- Extensive triggering capability
- Extensive protection features such as open sense lead detect, over- and under-voltage and current, and over-temperature
- And my personal favorite: you can track power events by adding a black box recorder (N7908A). The N7908A Black Box Recorder is a user-installable option that performs continuous background logging of output voltage, current, power, and system status to its own dedicated mass storage device. Features of this option include:
- Automatic logging starts when the power supply is turned on
- Logs in a circular buffer of about 380 MB
- Select one record every 10 ms (24 hours of logging) or one record every 100 ms (10 days of logging).
- Each record saves the average, maximum, and minimum values for voltage, current, and power in addition to power supply status bits and events
- Logged data is preserved after a power cycle. A time-stamped event is logged each time power is turned on.
The black box recorder is pretty cool, no? If you have a
mission critical power application, this option is a must to keep track of any
power related events that might affect your device under test.
One of my colleagues, Neil Forcier, posted about these
products on his GPETE blog earlier this month. Here is a link to that post: http://gpete-neil.blogspot.com/2013/09/the-new-advanced-power-system-designed.html
For more detailed information, take a look at the datasheet:
http://cp.literature.agilent.com/litweb/pdf/5991-2698EN.pdf
The datasheet contains some fantastic details about the
products including 9 tests challenges that are directly addressed by these
powerful products. In fact, you can read about each of the 9 test challenges
here: www.agilent.com/find/TestChallenges
With all of these advanced features built into this family
of products, I think you can now appreciate why we called it the Advanced Power
System!
Friday, September 27, 2013
New Agilent Autoranging Power Supplies provide Higher Power
I have stated before that I avoid posting product-only-focused material in this blog since our intention here is to educate about all-things-power rather than to (directly) promote our products. But when we (Agilent….for now…) come out with new power products, I think it is appropriate for me to announce them here. The last time I did this was back on January 23, 2012 in this post:
Coincidentally, those products were autoranging power supplies just like some of the power products we just introduced! Earlier this month, Agilent announced two new families of high-power system power supplies with this press release:
The two new families are the:
· N6900/N7900 Series 1- and 2-kW Advanced Power System (APS) DC Power Supplies
· N8900 Series 5-, 10-, and 15-kW Autoranging DC Power Supplies
Today I will focus on the higher power series, the N8900. Next week, I’ll post about the N6900/N7900 series.
What is particularly exciting for us about the N8900 series of products is that it is the highest power level we have ever provided. I’ve been working here at Agilent with power products since 1980 (we were Hewlett-Packard back then and will soon get yet another new name), and until now, the highest-power power supply we offered was the HP SCR-10 Series at 10 kW. This product was discontinued many years ago. Now the new N8900 series has 5, 10, and 15 kW in a single model and outputs can be paralleled for 100 kW or more! Now that’s a lot of power!!
Back when I started, 10 kW came in a much larger package and weighed over 500 lb (227 kg)! Today, we can get 50% more power (15 kW total) in an 80% smaller package (3 U vs 16 U) that is 85% lighter (73 lb vs 500 lb). See the figure below.
The new N8900 series offers 14 different voltage, current, and power combinations with output voltages up to 1500 V and output currents up to 510 A. Outputs can be put in parallel for 100 kW or more. These are basic power supplies, but have autoranging output characteristics so you get more voltage and current combinations from a single output than if you used a power supply with a rectangular output characteristic. See the figure below.
For more information about autorangers and output characteristics, see the post I mentioned earlier (or click here.)
We also created a video introducing the N8900 series (I do a cameo toward the end…can you pick me out?).
These basic power supplies will be used in many different high-power applications, such as hybrid-electric vehicle test and photo-voltaic inverter test. So if you need a basic high-power power supply, check out the Agilent N8900 Series. And don’t hesitate to ask me a question about the product or its suitability for your application.
Labels:
10 kW,
100 kW,
15 kW,
5 kW,
high power,
N8900,
power supply,
SCR-10,
Usage
Subscribe to:
Posts (Atom)