As I mentioned in a previous post, we have devoted a lot of time writing about protecting your device under test (DUT) from the two main DUT-destroying forces available from a power supply: excessive voltage and excessive current. Click here for one of the latest posts including a list to the other posts.
Today I’d like to cover another topic that can cause DUT failure due to a power supply. Some DUTs have multiple DC inputs and some of these multiple-input DUTs are sensitive to the order in which the inputs turn on or turn off. Subjecting the device to an uncontrolled sequence could cause latch-up or excessive current to flow resulting in compromised reliability or even immediate catastrophic failure of the DUT. So properly sequencing the multiple voltages at turn on and off is essential. My colleague, Ed Brorein, wrote a very similar post last year (click here) but I thought this topic was worth repeating especially since we added another series of power products with higher power that has this capability.
Various methods have been used in an effort to address the potential problem associated with improperly sequenced power inputs. Diodes can be placed from one input to another to clamp the voltage thereby preventing one input voltage from going too far above or below another input voltage but this method has limited effectiveness and variable results. Relays can be put in series with each input and controlled with timing circuitry but the relays introduce variable series impedance and timing is imprecise. FETs with associated control circuitry can be placed in series with each input however this method requires significant design time and adds complexity to the setup. Multiple DC power supplies can be controlled through software, but once again, timing is imprecise and response times can be slow.
Several years ago, I wrote an application note on a closely related topic (click here). The method that is most precise and introduces the fewest complications is to use a power supply system that has output sequencing integrated into the system itself. Keysight has several power supply systems that can accommodate precise output sequencing: the N6700 Modular Power System, N6705 DC Power Analyzer, and the more recently released N6900/N7900 Advance Power System. Each system offers the ability to precisely control the turn-on and turn-off sequence of multiple outputs. Timing is set with sub-millisecond resolution. Synchronization across systems is also possible to facilitate timed shut downs of larger numbers of power supply outputs for your DUT inputs. The above mentioned application note specifically addressed the topic of how to configure the system to properly shut down your DC inputs in sequence upon a fault generated by any of the system power supplies.
Below is a simple example of a sequenced turn on of four outputs in an N6705B mainframe. The sequencing is facilitated by setting a different turn-on delay time for each of the outputs (turn-off delays can be set independently). When all outputs are told to turn on simultaneously, the delays are activated resulting in a precisely controlled sequenced turn on. Figure 1 shows how easy it is to implement the delays for a turn-on event. In this case, I used four power supply outputs in an N6705B mainframe with delays set to 5 ms, 10 ms, 15 ms, and 20 ms. I set the output voltages to 10 V, 7.5 V, 5 V, and 3.3 V. You can also set the output voltage rise time (slew rate) independently for each output. Figure 2 shows the results using the scope that is built into the N6705B mainframe.
So you can see that with the proper power supply system, sequencing your multiple DC power supply inputs on your device to protect it from damage is easy. Keysight provides you with the solution to do just that adding to our arsenal of features that protect your valuable DUT.
Monday, September 29, 2014
Wednesday, September 17, 2014
Simulating battery contact bounce, part 1
One test commonly done during design validation of
handheld battery powered devices is to evaluate their ability to withstand a
short loss of battery power due to being bumped and the contacts momentarily
bouncing open, and either remain operating or have sufficient time to handle a shutdown
gracefully. The duration of a contact bounce can typically range anywhere from
under a millisecond to up to 100 milliseconds long.
To simulate battery contact bouncing one may consider
programming a voltage drop out on a reasonably fast power supply with arbitrary
waveform capabilities, like several of the N675xA, N676xA, or N678xA series
modules used in the N6700 series Modular DC Power System or N6705B DC Power
Analyzer mainframe, shown in Figure 1. It is a simple matter to program a
voltage dropout of specified duration. As an example a voltage dropout was
programmed in Figure 2 on an N6781A SMU module using the companion 14585A
software.
Figure 2: Programming a voltage drop out using the N6705B
and N6781A SMU module
While a voltage dropout is fine for many applications,
like automotive, in many situations it does not work well for simulating
battery contact bounce. The reason for this is there is one key difference to
note about a voltage dropout versus a battery contact bounce. During a voltage
dropout the source impedance remains low. During a battery contact bounce the
source impedance is an open circuit. However, a DC source having the ability to
generate a fast voltage dropout is a result of it being able to pull its output
voltage down quickly. This is due to its ability to sink current as well as
source current. The problem with this is, for many battery powered devices,
this effectively short-circuits the battery input terminals, more than likely
causing the device to instantly shut down by discharging any carry-over storage
and/or disrupting the battery power management system. As one example consider
a mobile device having 50 microfarads of input capacitance and draws 4
milliamps of standby current. This capacitance would provide more than adequate
carryover for a 20 millisecond battery contact bounce. However, if a voltage
dropout is used to simulate battery contact bounce, it immediately discharges
the mobile device’s input capacitance and pulls the battery input voltage down
to zero, as shown by the red voltage trace in Figure 3. The yellow trace is the
corresponding current drain. Note the large peaks of current drawn that
discharge and recharge the DUT’s input capacitor.
One effective solution for preventing the DC source from
shorting out the battery input is to add a DC blocking diode in series with the
battery input, so that current cannot flow back out, creating high impedance
during the dropout. This is illustrated in Figure 4.
Figure 4: Blocking diode added between SMU and DUT
One thing to note here is the diode’s forward voltage
drop needs to be compensated for. Usually the best way to do this just program
the DC source with the additional voltage needed to offset the diode’s voltage
drop. The result of this is shown in Figure 5. As shown by the red trace the
voltage holds up relatively well during the contact bounce period. Because the
N6781A SMU has an auxiliary voltage measurement input it is able to directly
measure the voltage at the DUT, on the other side of the blocking diode,
instead of the output voltage of the N6781A. As seen by the yellow current
trace there is no longer a large peak of current discharging the capacitor due
to the action of the blocking diode.
Now you should have a much better appreciation of the
differences between creating a voltage dropout and simulating battery contact
bounce! And as can be seen a blocking diode is a rather effective means of
simulating battery contact bounce using a voltage dropout. Stay tuned for my
second part on additional ways of simulating battery contact bounce on an
upcoming posting.
.
Wednesday, September 10, 2014
How do I protect my DUT against my power supply sense lines becoming disconnected, misconnected, or shorted?
The remote sense lines are a vital part of any good
system power supply. As shown in Figure 1, by using a second, separate pair of leads
for sensing, the output voltage is now regulated right at the DUT rather than
at the output terminals on the power supply. Any voltage drops in the force
leads are compensated for; assuring the highest possible voltage accuracy is
achieved right at the DUT.
Figure 1: Remotely sensing and regulating output voltage
at the DUT
Of course for this to work correctly the sense leads need
to have a good connection at the DUT. However, what if the sense leads become
disconnected, misconnected, or shorted?
One might think if one or both of the sense leads became
disconnected, the sensed voltage would then become zero, causing the output
voltage on the force leads to climb up out of control until the over voltage
protect (OVP) trips. This turns out not to be the case, as a co-contributor
here, Gary had pointed out in a previous posting “What happens if remote sense
leads open?” (Click here to review). Basically a passive protection mechanism
called sense protect maintains a backup connection between the sense line and
corresponding output terminal inside the power supply in the event of a sense
line becoming disconnected.
While sense protect is an indispensable feature to help
protect your DUT by preventing runaway over-voltage, if a sense lead is open
the voltage at your DUT is still not as accurate as it should be due to
uncompensated voltage drops in the force leads. This can lead to miscalibrated
DUTs and you would not even know that it is happening. To address this some
system power supplies include an active open sense lead fault detection system.
As one example our 663xx Mobile Communications DC Sources check the sense lead
connections during each output enable and will issue a fault protect and shut
down the output if one or both sense leads become disconnected. It will also
let you know which of the sense leads are disconnected. It can be enabled and
disabled as needed. I had written about this in a previous posting “Open sense
lead detection, additional protection for remote voltage sensing” (Click here to review).
Taking sense protection further, we have incorporated a
system we refer to as sense fault detect (SFD) in our N6900A and N7900A
Advanced Power System (APS). It can be enabled or disabled. When enabled it
continually monitors the sense lead connections at all times. If it detects a
sense fault it sets a corresponding bit in the questionable status group
register as well as turn on status annunciator on the front panel to alert the
user, but does not disable the output. Through the expression signal routing
system a “smart trigger” can be configured as shown in Figure 2 to provide a
protect shutdown on the event of a sense fault detection. In all, sense fault detect on APS provides a
higher level of protection and flexibility.
Figure 2: Configuring a custom opens sense fault protect
on the N6900/N7900 APS
What happens if the sense leads become shorted? Unlike
open sense leads, in this case the output voltage can rise uncontrolled. The
safeguard for this relies on the over voltage protect system. The same thing
happens if the sense leads are reversed. The power supply will think the output
voltage is too low and keep increasing the output voltage in an attempt to
correct it. Again the safeguard for this relies on the over voltage protect
system. The N6900/N7900 APS does actually distinguish the difference when the
sense leads are reversed by generating a negative OVP (OV-) fault, giving the
user more insight on what the fault is to better help in rectifying the
problem.
Remote voltage sensing provides a great benefit by being
able to accurately control the voltage right at the DUT. Along with the
appropriate safeguards against sense lead misconnections you get all the
benefit without any of the corresponding risks!
Labels:
APS,
fault protection,
load lead drop,
miswires,
open remote sense leads,
open sense lead detect,
open sense lead protect,
remote sense,
reversed sense leads,
shorted sense leads,
tracking OVP,
Usage
Sunday, August 31, 2014
How do I transfer files from my DC Power Analyzer to my PC?
Hi everybody!
I got back from my vacation just in time to get my August blog post out. We typically try to shy away from product specific blog postings here at Watt's Up but this is a topic that I get a bunch of questions on in my support job and this is a great place for me to address it.
The Keysight N6705B DC Power Analyzer has an internal flash drive that stores information such as datalogs and scope waveforms. When we first came out with the N6705B, it had a 64 MB drive (it is crazy how small that seems today). Present N6705Bs have a 4 GB drive in them. Since you can create datalogs of up to 2 GB in size, even a 4 GB drive can get full. Today I am going to talk about how to get a file out of the internal drive of the N6705B and onto your PCs hard drive.
The way that I see it, there are three ways to get a file off the N6705B:
I got back from my vacation just in time to get my August blog post out. We typically try to shy away from product specific blog postings here at Watt's Up but this is a topic that I get a bunch of questions on in my support job and this is a great place for me to address it.
The Keysight N6705B DC Power Analyzer has an internal flash drive that stores information such as datalogs and scope waveforms. When we first came out with the N6705B, it had a 64 MB drive (it is crazy how small that seems today). Present N6705Bs have a 4 GB drive in them. Since you can create datalogs of up to 2 GB in size, even a 4 GB drive can get full. Today I am going to talk about how to get a file out of the internal drive of the N6705B and onto your PCs hard drive.
The way that I see it, there are three ways to get a file off the N6705B:
- The old fashioned way: You use a thumb drive and manually transfer the files that way. The disadvantage here is that you need to have a thumb drive and there is no way to automate the process.
- You can use the N6705B LXI web interface. There's a utility there that can transfer files bwtween the N6705B and your PC. The disadvantages of this are that you cannot automate it and you can only do this if you are connected via LAN.
- There is a command (MMEM:DATA?) that will read back the contents of a file so you could write a SCPI program to do this. This disadvantage here is that you need to write a program. Luckily, I have done this in the past myself and I am more than willing to help!
As you can see in the program, I basically read the contents of the file default.dlog into filedata which I have dimensioned as a byte array. After I read all the data in, I kill any null data in the array and then copy it into a file that I have stored on my hard drive. All in all, if you use this method it is pretty easy.
That's all I have for this month. Please let me know if you have any questions or if you have discovered another way to transfer files.
Thursday, August 28, 2014
What can cause a power supply output voltage to exceed its setting?
We have done a number of posts on power supply protection topics covering both voltage and current issues:
Safeguarding your power-sensitive DUTs from an over power condition
How does power supply overvoltage protection work?
Protect your DUT from over-current in more ways than one
What is a power supply’s over current protect (OCP) and how does it work?
Overvoltage protection: some background and history
Protect your DUT: use sense leads for overvoltage protection (OVP)
Types of current limits for over-current protection on DC power supplies
Protect your DUT with power supply features including a watchdog timer
And just last week, on August 20, 2014, my colleague and fellow Watt’s Up? blog contributor, Ed Brorein, presented a live webcast called “Protect Your Device Against Power-Related Damage During Test” which was recorded and can be accessed here. Before he presented the seminar, Ed mentioned it here.
Many of these posts talked about how the power supply responds to an overvoltage or overcurrent condition. Today I want to talk about what causes an overvoltage condition. I’m defining an overvoltage condition as a condition that causes the power supply output voltage to exceed its setting. Let’s take a look at some of the things that can cause this to happen.
Causes of power supply output voltage exceeding its setting
User-caused miswires
These miswires should be found and corrected during test setup verification before a device under test (DUT) is connected to the power supply. Possible miswires and their effect on the power supply output voltage are:
Safeguarding your power-sensitive DUTs from an over power condition
How does power supply overvoltage protection work?
Protect your DUT from over-current in more ways than one
What is a power supply’s over current protect (OCP) and how does it work?
Overvoltage protection: some background and history
Protect your DUT: use sense leads for overvoltage protection (OVP)
Types of current limits for over-current protection on DC power supplies
Protect your DUT with power supply features including a watchdog timer
And just last week, on August 20, 2014, my colleague and fellow Watt’s Up? blog contributor, Ed Brorein, presented a live webcast called “Protect Your Device Against Power-Related Damage During Test” which was recorded and can be accessed here. Before he presented the seminar, Ed mentioned it here.
Many of these posts talked about how the power supply responds to an overvoltage or overcurrent condition. Today I want to talk about what causes an overvoltage condition. I’m defining an overvoltage condition as a condition that causes the power supply output voltage to exceed its setting. Let’s take a look at some of the things that can cause this to happen.
Causes of power supply output voltage exceeding its setting
User-caused miswires
These miswires should be found and corrected during test setup verification before a device under test (DUT) is connected to the power supply. Possible miswires and their effect on the power supply output voltage are:
- Shorted sense leads – the output voltage will rapidly rise above the setting. Keysight power supplies will prevent the output from rising above the overvoltage protection (OVP) setting.
- Reversed sense leads – on most power supplies, the output voltage will rapidly rise above the setting and on Keysight supplies, it will be stopped by the OVP circuit. On our N6900/N7900 Advanced Power System (APS) power supplies, this condition is caught sooner: OV- is triggered when the output reaches about 10% of the rated voltage, so the output does not have to rise to the setting and above.
- Open sense leads – If your power supply does not have protection for open sense leads, it is possible for your output to rapidly rise above the setting if one or both sense leads are open. Keysight power supplies have built-in sense protect resistors which limit the output voltage rise to about 1% above the setting. The voltage will continue to be regulated there. In addition to limiting the output to about 1% above the setting with an open sense lead, Keysight N6900/N7900 APS power supplies have a feature called open sense lead detection. When enabled, open sense lead detection will cause a sense fault (SF) status about 50 us after open sense leads are detected. This status does not turn off the output, but it can be configured to turn off the output using the advanced signal routing capability.
- Special note about N7900 power supplies (not N6900): these models have output disconnect relays that open upon a protection fault. These mechanical relays take about 20 ms to open. Before they open, the output downprogrammer circuit is activated for about 2 ms and draws about 10% of rated output current to reduce the output voltage. The N7976A and N7977A (both higher voltage models) also have solid state relays in series with the mechanical relays. Upon a protection fault on these 2 models, the downprogrammer activates for 2 ms followed immediately by the solid state relays opening and then the mechanical relays open about 20 ms later.
Inadvertent wiring failure
- Sense leads inadvertently become shorted – power supply response is the same as mentioned above under shorted sense leads
- Sense leads inadvertently become open – power supply response is the same as mentioned above under open sense leads
- Sense leads should never become inadvertently reversed, nevertheless, the power supply response is the same as mentioned above under reversed sense leads
Power supply fault (circuit failure)
Note that Keysight’s overall power supply failure rate is very low. Since the below mentioned failures are a subset of all failures, they are very rare. This means that failures that cause the output to go to a higher-than-desired value are a small percent of a small percent, and while not impossible, they are extremely unlikely events.
- Power element fails (shorts)
- Series regulator – when a series regulator power element shorts, the output very quickly rises above the rated voltage of the power supply. The only way to limit this is to trip OVP and either fire an SCR across the output to bring the voltage back down or open output relays. For example, the Keysight N678xA models use a series regulator. When OVP trips on N678xA models, output relays are opened to protect the DUT. Solid state relays very quickly open first followed by mechanical relays about 6 ms later.
- Switching regulator – when a Keysight switching regulator power element shorts, the output will go toward zero volts instead of rising since Keysight switching regulators use power transformers and no power can be transferred through the transformer without the switching elements turning on and off. For example, all N6700 and N6900/N7900 series models use switching regulators except the N678xA models (series regulators).
- Note that if a power element fails open using either power regulation scheme, the output voltage will fall, not rise, so this condition is not a concern when looking at excessive output voltage possibilities.
- Regulation circuit failure (bias supply, DAC, amplifier, digital comparison processor, etc.)
- There are various circuits that could fail and cause the output voltage to rise in an uncontrolled manner. Keysight power supplies have OVP designed to respond to these failures. In series regulators, an SCR across the output can fire to reduce the voltage or output relays can open. In switching regulators, the pulse width modulator is turned off to prevent power from flowing to the output, downprogrammers are activated to pull any excessive voltage down, and output relays are opened (when present) to disconnect the output from the DUT.
- Multiple parallel failures – if both a regulating circuit fails that causes the output to rise AND the OVP circuit fails, there would be nothing to prevent the output voltage from rising above the setting. While this is possible, it requires just the right combination of multiple circuit failures and is therefore extremely unlikely.
Output response to load current transients
- It is possible for the output voltage to temporarily rise above the setting for short transients in response to fast load current changes (especially unloading). If the voltage excursion is high enough and long enough, it is possible that the OVP will activate and respond as outlined above.
External power source
- It is possible for an external source of power (such as a battery, charged capacitor, inductor with changing current, or another power supply) to cause the voltage to go above the setting. The OVP will respond to this condition as outlined above. If the external power source can provide more current than the rating of the power supply and an SCR circuit is used in the power supply, it is prudent to put a fuse in series with the external source of power to prevent damage to the power supply SCR and/or output circuit from excessive current.
So you can see that there are a number of ways in which the output voltage can rise above the setting. Luckily, Keysight design engineers are aware of these possibilities and have lots of experience adding protection circuits to prevent damage to your DUT!
Labels:
Design,
miswires,
open remote sense leads,
open sense lead detect,
open sense lead protect,
overvoltage,
overvoltage protection,
OVP,
power supply,
reversed sense leads,
shorted sense leads
Wednesday, August 20, 2014
Some differences between constant current (CC) and constant resistance (CR) loading on your DUT’s performance
Most electronic loads provide constant current (CC),
constant resistance (CR) and constant voltage (CV) loading. Some also offer
constant power (CP) loading as well. The primary reason for this is this gives
the test engineer a choice of loading that best addresses the loading
requirement for the DUT, which invariably is some kind of power source.
Most usually the device should be tested with a load that
reflects what the loading is like for its end use. In the most common case of a
device being predominantly a voltage source the most common loading choices are
either CC or CR loading, which we will look at in more detail here. Some feel
they can be used interchangeably when testing a voltage source. To some extent
this is true but in some cases only one or the other should be used as they can impact
the DUT’s performance quite differently.
Let’s first consider static performance. In Figure 1 we
have the output characteristics of an ideal voltage source with zero output
resistance (a regulated power supply, for example) and a non-ideal voltage
source having series output resistance (a battery, for example). Both have the same open circuit (no load) voltage.
Superimposed on these two source output characteristics are two load lines; one
for CC and one for CR. As can be seen they are set to draw the same amount of
current for the ideal voltage source. However, for the non-ideal voltage
source, while the CC load still continues to draw the same amount of current in spite of the voltage drop,
not surprisingly the CR load draws less current due to its voltage-dependent
nature.
Figure 1: CC and CR loading of ideal and non-ideal
voltage sources
CC loading is frequently used for static power supply
tests for a key reason. Power supplies are usually specified to have certain
output voltage accuracy for a fixed level of current. Using CC loading assures the
loading condition is met, regardless of power supply’s output voltage being low
or high, or in or out of spec. Non-ideal voltage sources, like batteries,
present a little more of a problem and are often specified for both CC and CR
loading as a result, to reflect the nature of the loading they may be subjected
to in their end use. Due to a battery's load-dependent output voltage, trying to use one type of loading in place the other becomes
an iterative process of checking and adjusting loading until the acceptable operating
point is established.
Let’s now consider dynamic performance. CC loading generally has a greater impact on a
power supply’s ability to turn on as well as its transient performance and
stability, in comparison to CR loading. When the power supply first starts up
its output voltage is at zero. A CR load would demand zero current at start up.
In comparison a CC load still demands full current. Some power supplies will
not start up properly under CC loading. With regard to transient response and
stability, CR loading provides a damping action, increasing current demand when
the transient voltage increases and decreases demand when the transient voltage
decreases, because the current demand is voltage dependent. CC loading does not
do this, which can negatively influence transient response and stability
somewhat. Whether CC or CR loading is used depends on what the power supply’s
specifications call out for the test conditions. Batteries have some dynamic
considerations as well. Their output response can be modeled as a series of
time constants spanning a wide range of time. This presents somewhat of a
moving target for an algorithm that uses an iterative approach to settling on
an acceptable operating point.
This is just a couple of examples of how a load’s
characteristic affects the performance of the device it is loading, and why electronic
loads have multiple operating modes to select from, and worth giving thought next
time towards how your device is affected by its loading!
Tuesday, August 5, 2014
Upcoming Seminar on Protecting Your Device against Power-Related Damage during Test
Here on “Watt’s Up?” we have provided a good number of
posts about various protection features incorporated into system power supplies
to protect your device against power-related damage during test. Just recently
my colleague Gary posted “How Does Power Supply Over-Voltage Work?” (Click here to review) Here he reviews inner workings of different OVP implementations. I recently posted “Safeguarding Your
Power-Sensitive DUTs against an Over-Power Condition” (Click here to review) Here I go
over a method to protect your DUT against excess power when other power supply
features like over current protection may be less than ideal.
The reason why we frequently share power-related
protection topics here is protecting your DUT is extremely important, there are
a lot of different capabilities incorporated in system power supplies for this
purpose, and there are a lot of practical considerations when putting them to
use.
Hopefully a number of you have found our posts on
protection-related topics of help. Because this is a very important topic and
there is so much more you should know about it I will be giving a live
web-based seminar “Protecting Your Device against Power-Related Damage during
Test” on August 20th, just a few weeks away from today. I will be
going over a number of protection-related topics which we have not yet covered
here on “Watt’s Up?”. One of my
objectives is to provide a more holistic view of the many ways a system power
supply is able to better safeguard against power-related damage as well as what
is practical to expect when using these various capabilities incorporated in
the power supply.
You can register online at the following (Click here for description and registration page) In case you are not able to attend the live event on August 20 you will
be able to register and listen to seminar afterward as well, as it will be
recorded.
So if protecting your device against power-related damage
is important to you I hope you are able to attend the seminar!
Labels:
discrete fault indicator,
fault protection,
OCP,
open sense lead detect,
open sense lead protect,
over voltage protect,
over-current protection,
OVP,
power supply protection,
remote inhibit,
Usage
Subscribe to:
Posts (Atom)