Hello everyone!
Happy New Year! This is our last post of 2014 so we wanted to wish all of our readers a Happy New Year. Today I am going to talk about a question that I have been asked a few times lately. In many of our power supplies, we list our Programming Resolution as an average number. Many people want to know why we do it this way.
Look at the below snippet from our 664xA DC Power Supplies Supplemental Characteristics:
You can see that that it is clearly stated as an average.
The simple answer to this question is that this is because of calibration.
The more complex answer is that we use a DAC to control the output setting of the power supply. A certain number of DAC counts is going to represent zero to full scale on the output of the supply. For simplicity's sake, lets assume that we are using a 12 bit DAC for a power supply that goes to fifty volts.
In an ideal world where calibration is not necessary:
A 12 bit DAC gives us 2^12 or 4096 total counts.
The step size (programming resolution) of the 50 volt power supply would be 50/4096 or 0.0122 volts.
We do not live in an ideal world though so we have to disregard some DAC counts because of how the unit calibrates. We also generally let you program a little bit above the maximum settings (usually something like 2%). Zero volts is not going to be zero DAC Counts and 50 V is not going to be 4096 DAC counts. For our example, lets say that the minimum that we disregard 20 counts at the top and bottom (40 total counts) and the maximum we disregard is 120 counts (240 total counts) at the top and bottom. In this scenario:
Minimum step size = 50/(4096-40) = 0.0123 V
Maximum step size = 50/(4096-120) = 0.0130 V
For our Supplemental Characteristic, we would take the average of those 2 numbers. This gives us 0.01265 V.
The big question is how would I know what the programming resolution is for my particular unit. I spent about half of yesterday trying to figure that out and I'm still working that out myself. The best solution that I have right now is to hook a DMM to the output and slowly increment my output to see when it flips to a new setting. I need to experiment on this though. If any readers have a better idea, please let us know in the comments. The fact of the matter is that the error is pretty small and to be safe, any error due to being in between DAC counts is included in our Programming Accuracy specification.
Well that is all for 2014. I hope that everyone has a safe and happy 2015. See you next year!
Matt
Wednesday, December 31, 2014
Tuesday, December 30, 2014
Why does an electronic load draw a pulse of current when a voltage is initially applied?
We recently had a customer contact us about one of our electronic loads. He had a solid state switch in series with a fixed output voltage source (for example, 50 V) and set the load to a fixed current (for example, 1 A). He used a current probe and a scope to observe the current flowing into the electronic load. When the switch changed from open to closed he saw a pulse of current flowing into the load that was significantly higher than the load set value before the load settled to the set value of 1 A. He was wondering if this was normal. It is normal. Here’s why:
The electronic loads have a snubber network across their input terminals. The snubber typically consists of a resistor in series with a capacitor. For example, the Keysight N3304A electronic load has 2.2 uF in series with about 2 ohms. The snubber network is there to maintain stability on the load input for all settings and operating modes. When the customer’s switch was closed, the initially discharged capacitor in the snubber pulled a pulse of current to begin charging. If the dV/dt of the load input voltage waveform was infinitely fast, the cap would initially look like a short and the initial current pulse would be limited by the resistor as I = V/R. In this example, the current pulse would have been 50 V / 2 ohms = 25 A. But he was seeing a much smaller current pulse: around 2.4 A instead of 25 A, but still higher than the expected set value of 1 A. This means the dV/dt was not infinite (the solid state switch had a finite risetime). In this case, the current pulse would be limited by the dV/dt of the input voltage waveform.
As an example, see Figure 1 below showing the input voltage and input current for an N3304A load. The voltage rises from 0 V to 50 V over about 75 us and the fastest part of the risetime is about 1V/us. Since I = C dV/dt, and for this electronic load, C = 2.2 uF, the peak of the current is calculated to be 2.2 uF x 1V/us = 2.2 A. The plot shows it to be about 2.4 A, so this is close to the expected peak value. As the dV/dt of the input voltage slows down, the current drops from its peak and approaches zero amps as the dV/dt slows to zero (horizontal). (Note that in the plot below, the load was set for zero current.)
The electronic loads have a snubber network across their input terminals. The snubber typically consists of a resistor in series with a capacitor. For example, the Keysight N3304A electronic load has 2.2 uF in series with about 2 ohms. The snubber network is there to maintain stability on the load input for all settings and operating modes. When the customer’s switch was closed, the initially discharged capacitor in the snubber pulled a pulse of current to begin charging. If the dV/dt of the load input voltage waveform was infinitely fast, the cap would initially look like a short and the initial current pulse would be limited by the resistor as I = V/R. In this example, the current pulse would have been 50 V / 2 ohms = 25 A. But he was seeing a much smaller current pulse: around 2.4 A instead of 25 A, but still higher than the expected set value of 1 A. This means the dV/dt was not infinite (the solid state switch had a finite risetime). In this case, the current pulse would be limited by the dV/dt of the input voltage waveform.
As an example, see Figure 1 below showing the input voltage and input current for an N3304A load. The voltage rises from 0 V to 50 V over about 75 us and the fastest part of the risetime is about 1V/us. Since I = C dV/dt, and for this electronic load, C = 2.2 uF, the peak of the current is calculated to be 2.2 uF x 1V/us = 2.2 A. The plot shows it to be about 2.4 A, so this is close to the expected peak value. As the dV/dt of the input voltage slows down, the current drops from its peak and approaches zero amps as the dV/dt slows to zero (horizontal). (Note that in the plot below, the load was set for zero current.)
So you can see that the current flowing into the input of an electronic load may not be simply the DC setting you expect. If you apply a dynamic voltage waveform to the input, the RC snubber network will also draw some current for a short time until the voltage applied to the load input stabilizes. There is another factor involved here that is worth mentioning but I will not cover in detail in this post since it is a secondary effect in this case. In this customer’s situation, the load was set for 1 A and initially had no voltage on it (his solid state switch was open). The load was trying to draw current by turning on its input FETs, but there was no voltage applied, so the load went to an unregulated state. When the voltage finally appeared (the solid state switch was closed), the FETs that were turned on hard had to recover and take a finite amount of time to begin regulating the set current. This effect can also contribute to brief, temporary unexpected current draw by the load when a voltage is suddenly applied to the input.
Friday, December 12, 2014
Why Does Over Current Protect (OCP) have a Programmable Delay Value in the First Place?
Since I am on a roll about over current protect (OCP),
having just completed a two-part posting “Why does the response time of OCP
vary on the power supply I am using and what can I do about it?” (Review part 1) (Review part 2) there is yet another aspect about OCP that is worth bringing
up at this time. And that is “why does OCP have a programmable delay value in
the first place?” This actually came up in a discussion with a colleague here
after having read my part posting.
It may seem a bit ironic that OCP has a programmable
delay in that in my posting on OCP I shared ideas on how one can minimize the response
time delay encountered. But this is not contradictory. One may very well want
to minimize it, eliminating extra delay being encountered, but not necessarily eliminate
it altogether. As can be seen in my previous postings, I had programmed the OCP
delay time to 5 ms.
The programmable OCP delay does serve a purpose, and that
is to prevent false OCP trips. Adding some delay time prevents these false
trips. For someone who knows the root
cause of false OCP tripping they might be half right. There are actually been
two main causes of false OCP trips which are prevented by adding some delay
time.
The original problem with
OCP was that it would be falsely tripped when output voltage settings were
changed on the power supply, due to capacitive loading at the test fixture or
within the DUT. This is especially prominent with inrush current when first
bringing up the voltage to power the DUT. An OCP delay prevents false
triggering under these conditions. To correct the false tripping the delay would
be invoked when output programming changes were made. As one example, the OCP
delay description in our manual for our 663x series power supplies states:
“This command sets the time between the
programming of an output change that produces a constant
current condition (CC) and the
recording of that condition by the Operation Status Condition register. The
delay prevents the momentary changes
in status that can occur during reprogramming from being
registered as events by the status
subsystem. Since the constant current condition is used to trigger
overcurrent
protection (OCP), this command also delays OCP.”
Under this situation the momentary overcurrent is induced
by the power supply. Although not nearly as much as in issue in practice,
momentary overcurrents can also be DUT-induced as well. This is the second
situation that can cause a false tripping of the OCP. The DUT may be
independently turned on after the bias voltage has already been on and draw a
surge of current. Or the DUT may change mode of operation and draw a temporary
surge of current. If the OCP delay is
invoked only by an output programming change it does not have any effect in
these situations.
On later generation products, such as our N6700, N6900,
and N7900 series, the user also has the ability to programmatically select
between having the OCP delay activate from either an output change, or from
going into CC condition. This gives the user a way to remain consistent with
original operation or have OCP delay effective for momentary DUT-induced
overload currents as well!
Labels:
APS,
current limit,
fault protection,
inrush current,
OCP,
over-current protection,
Usage
Friday, December 5, 2014
Why does the response time of OCP vary on the power supply I am using and what can I do about it? Part 2
In the first part of this posting (click here to review) I
highlighted what kind of response time is important for effective over current
protection of typical DUTs and what the actual response characteristic is for a
typical over current protect (OCP) system in a test system DC power supply. For
reference I am including the example of OCP response time from the first part
again, shown in Figure 1.
Figure 1: Example OCP system response time vs. overdrive
level
Here in Figure 1 the response time of the OCP system of a
Keysight N7951A 20V, 50A power supply was characterized using the companion
14585A software. It compares response times of 6A and 12A loading when the
current limit is set to 5A. Including the programmed OCP delay time of 5
milliseconds it was found that the actual total response time was 7
milliseconds for 12A loading and 113 milliseconds for 6A loading. As can be seen, for reasons previously
explained, the response time clearly depends on the amount of overdrive beyond
the current limit setting.
As the time to cause over current damage depends on the
amount of current in excess of what the DUT can tolerate, with greater current
causing damage more quickly, the slower response at lower overloads is
generally not an issue. If however you
are still looking how you might further improve on OCP response speed for more
effective protection, there are some things that you can do.
The first thing that can be done is to avoid using a
power supply that has a full output current rating that is far greater than
what the DUT actually draws. In this way the overdrive from an overload will be
a greater percentage of the full output current rating. This will normally
cause the current limit circuit to respond more quickly.
A second thing that can be done is to evaluate different
models of power supplies to determine how quickly their various current limit
circuits and OCP systems respond in based on your desired needs for protecting
your DUT. For various reasons different models of power supplies will have
different response times. As previously discussed in my first part, the slow
response at low levels of overdrive is determined by the response of the
current limit circuit.
One more alternative that can provide exceptionally fast
response time is to have an OCP system that operates independently of a current
limit circuit, much like how an over voltage protect (OVP) system works. Here
the output level is simply compared against the protect level and, once
exceeded, the power supply output is shut down to provide near-instantaneous
protection. The problem here is this is not available on virtually any DC power
supplies and would normally require building custom hardware that senses the fault
condition and locally disconnects the output of the power supply from the DUT.
However, one instance where it is possible to provide this kind of
near-instantaneous over current protection is through the programmable signal
routing system (i.e. programmable trigger system) in the Keysight N6900A and
N7900A Advanced Power System (APS) DC power supplies. Configuring this
triggering is illustrated in Figure 2.
Figure 2: Configuring a fast-acting OCP for the
N6900A/N7900A Advanced Power System
In Figure 2 the N7909A software utility was used to
graphically configure and download a fast-acting OCP level trigger into an
N7951A Advanced Power System. Although this trigger is software defined it runs
locally within the N7951A’s firmware at hardware speeds. The N7909A SW utility
also generates the SCPI command set which can be incorporated into a test
program.
Figure 3: Example custom-configured OCP system response
time vs. overdrive level
Figure 3 captures the performance of this
custom-configured OCP system running within the N7951A. As the OCP
threshold and overdrive levels are the same this can be directly compared to
the performance shown in Figure 1, using the conventional, current limit based
OCP within the N7951A. A 5 millisecond OCP delay was included, as before.
However, unlike before, there is now virtually no extra delay due to a current
limit control circuit as the custom-configured OCP system is totally
independent of it. Also, unlike before, it can now be seen the same fast
response is achieved regardless of having just a small amount or a large amount
of overdrive.
Labels:
14585A software,
Advanced Power System,
APS,
current limit,
N6900,
N6900A,
N7900,
N7900A,
N7906A,
OCP,
output disable,
OVP,
Usage
Saturday, November 29, 2014
Why do I measure voltage to earth ground on a power supply with a floating output?
Occasionally, one of our power supply users contacts us with a question about voltages measured from one of the power supply output terminals to earth ground (same as chassis ground). All of our power supply outputs are floating with respect to earth ground. See my previous post about this here. In that post, I stated that neither output terminal is connected to earth ground. To be more specific, no output terminal is connected directly to earth ground. We do have internal components, mainly resistors and capacitors, connected from each output terminal to earth ground. These components, especially the caps to ground, help mitigate issues with RFI (radio-frequency interference) and ESD (electrostatic discharge). They help prevent our power supplies from being susceptible to externally generated RFI and ESD, and also help to reduce or eliminate any internally generated RFI from being conducted to wires connected to the output terminals thereby reducing RFI emissions.
So even though our outputs are considered floating with respect to earth ground, there frequently is a DC path from at least one of our output terminals to earth ground. It is typically a very high value resistor, such as several megohms, but could be as low as 0.5 MΩ. This resistor acts as a bleed resistor to discharge any RFI or ESD caps to earth ground that could be charged to a high float voltage.
As an example of a power supply with a resistor to earth ground, the Keysight N6743A has 511 kΩ (~0.5 M) from the minus output terminal to earth ground. This resistor was responsible for the voltage measurements to earth ground observed and questioned by one of our power supply users. He was using this power supply in the configuration shown in Figure 1 and measured 9.7 Vdc from his common reference point to earth ground (again, same as chassis ground).
He understandably did not expect to measure any stable voltage between these points given that the output terminals are floating from earth ground. But once we explained the high impedance DC path from the minus output terminal to earth ground inside each power supply (see Figure 2), and the 10 MΩ input impedance of his DMM, the measurement made sense. The input impedance of the voltmeter (DMM) must be considered to accurately calculate the measured voltage. This is especially true when high impedance resistors are in the circuit to be measured.
Figure 3 shows the equivalent circuit which is just a resistor divider accounting for the 9.7 V measurement. (The exact calculation results in 9.751 V.) Notice that the voltage of the 28 V power supply does not impact this particular voltage measurement (but its resistor to ground does). If the user had measured the voltage from the plus output of the 28 V power supply to earth ground, both the 28 V supply and 20 V supply would have contributed to his measurement which calculates out to be 37.05 V (if you check this yourself, don’t forget to move the 10 MΩ resistor accounting for the different placement of the DMM impedance).
So you can see that even with power supply output terminals that are considered floating, there can still be a DC path to earth ground inside the supply that will cause you to measure voltages from the floating terminals to ground. As one of my colleagues always said, “There are no mysteries in electronics!”
So even though our outputs are considered floating with respect to earth ground, there frequently is a DC path from at least one of our output terminals to earth ground. It is typically a very high value resistor, such as several megohms, but could be as low as 0.5 MΩ. This resistor acts as a bleed resistor to discharge any RFI or ESD caps to earth ground that could be charged to a high float voltage.
As an example of a power supply with a resistor to earth ground, the Keysight N6743A has 511 kΩ (~0.5 M) from the minus output terminal to earth ground. This resistor was responsible for the voltage measurements to earth ground observed and questioned by one of our power supply users. He was using this power supply in the configuration shown in Figure 1 and measured 9.7 Vdc from his common reference point to earth ground (again, same as chassis ground).
He understandably did not expect to measure any stable voltage between these points given that the output terminals are floating from earth ground. But once we explained the high impedance DC path from the minus output terminal to earth ground inside each power supply (see Figure 2), and the 10 MΩ input impedance of his DMM, the measurement made sense. The input impedance of the voltmeter (DMM) must be considered to accurately calculate the measured voltage. This is especially true when high impedance resistors are in the circuit to be measured.
Figure 3 shows the equivalent circuit which is just a resistor divider accounting for the 9.7 V measurement. (The exact calculation results in 9.751 V.) Notice that the voltage of the 28 V power supply does not impact this particular voltage measurement (but its resistor to ground does). If the user had measured the voltage from the plus output of the 28 V power supply to earth ground, both the 28 V supply and 20 V supply would have contributed to his measurement which calculates out to be 37.05 V (if you check this yourself, don’t forget to move the 10 MΩ resistor accounting for the different placement of the DMM impedance).
So you can see that even with power supply output terminals that are considered floating, there can still be a DC path to earth ground inside the supply that will cause you to measure voltages from the floating terminals to ground. As one of my colleagues always said, “There are no mysteries in electronics!”
Monday, November 24, 2014
Prewired rack delivers up to 90 kW of single-output DC power
As I have mentioned before, I avoid posting product-only-focused material in this blog since our goal is to educate about power-related items rather than to directly promote Keysight products. But when something new comes out, I like to announcement it here.
A little over a year ago, Keysight (we were Agilent at the time) announced a new power supply family with high-power outputs up to 15 kW per output (see link here). These high-power autoranging DC power supplies with individual outputs up to 1500 V or 510 A can be paralleled for even more power. Paralleling outputs with these supplies is simplified since multiple outputs can be grouped to act as a single output and the current share bus enables multiple outputs to more equally share current. But there are other considerations when paralleling multiple units. Wiring the AC inputs and DC outputs together takes design time and assembly time. Integrating the units together physically in a rack also takes time and effort. Designing the system to ensure the safety of operators is also very important. So Keysight decided to offer a prewired rack to help you overcome the challenges associated with racking high-power supplies.
On November 11, 2014 (less than 2 weeks ago), we announced a prewired rack that combines up to six of the 15 kW N8900 series power supplies for total power up to 90 kW from a single output. You can choose from a variety of DC output combinations with voltages from 80 V to 1500 V and currents from 60 A to 3060 A. That’s a lot of current! The rack’s internal configuration makes the multiple outputs appear as a single output allowing you to communicate with just one power supply through LAN, GPIB, or USB (all standard in the system). Click here for the press release for this new system and here for additional system information.
Perhaps you are working in R&D or manufacturing on EV/HEV, alternative energy (fuel cells, solar, etc.), industrial DC motors, large UPS’s, electroplating, or any of the many other high-power application areas that need DC power up to 90 kW with voltages to 1500 V or currents to 3060 A. If so, and you want to spend your engineering resources on your core competencies instead of racking power supplies together, let Keysight help you with our new N8900 Series Rack System.
A little over a year ago, Keysight (we were Agilent at the time) announced a new power supply family with high-power outputs up to 15 kW per output (see link here). These high-power autoranging DC power supplies with individual outputs up to 1500 V or 510 A can be paralleled for even more power. Paralleling outputs with these supplies is simplified since multiple outputs can be grouped to act as a single output and the current share bus enables multiple outputs to more equally share current. But there are other considerations when paralleling multiple units. Wiring the AC inputs and DC outputs together takes design time and assembly time. Integrating the units together physically in a rack also takes time and effort. Designing the system to ensure the safety of operators is also very important. So Keysight decided to offer a prewired rack to help you overcome the challenges associated with racking high-power supplies.
On November 11, 2014 (less than 2 weeks ago), we announced a prewired rack that combines up to six of the 15 kW N8900 series power supplies for total power up to 90 kW from a single output. You can choose from a variety of DC output combinations with voltages from 80 V to 1500 V and currents from 60 A to 3060 A. That’s a lot of current! The rack’s internal configuration makes the multiple outputs appear as a single output allowing you to communicate with just one power supply through LAN, GPIB, or USB (all standard in the system). Click here for the press release for this new system and here for additional system information.
Perhaps you are working in R&D or manufacturing on EV/HEV, alternative energy (fuel cells, solar, etc.), industrial DC motors, large UPS’s, electroplating, or any of the many other high-power application areas that need DC power up to 90 kW with voltages to 1500 V or currents to 3060 A. If so, and you want to spend your engineering resources on your core competencies instead of racking power supplies together, let Keysight help you with our new N8900 Series Rack System.
Labels:
90 kW,
high power,
high power rack,
Misc.,
N8900,
power supply,
power supply rack
Tuesday, November 18, 2014
Why does the response time of OCP vary on the power supply I am using and what can I do about it? Part 1
In a previous posting of mine “Providing effective protection of your DUT against over voltage
damage during test”(click here to review), an important consideration for effective protection was to
factor in the response time of the over voltage protect (OVP) system. Due to
the nature of over voltage damage, the OVP must be reasonably fast. The
response time can typically be just a few tens of microseconds for a reasonably
fast OVP system on a higher performance system power supply to hundreds of
microseconds on a more basic performance system power supply. This response
time usually does not vary greatly with the amount of over voltage being
experienced.
Just as with voltage, system power supplies usually incorporate
over current protect (OCP) systems as well. But unlike over voltage damage,
which is almost instantaneous once that threshold is reached, over current takes
more time to cause damage. It also varies in some proportion to the current
level; lower currents taking a lot longer to cause damage. The I2t
rating of an electrical fuse is one example that illustrates this effect.
Correspondingly, like OVP, power supply OCP systems also
have a response time. And also like OVP, the test engineer needs to take this
response time into consideration for effective protection of the DUT. However, unlike OVP, the response time of an
OCP system is quite a bit different. The response time of an OCP system is
illustrated in Figure 1.
Figure 1: Example OCP system response time vs. overdrive
level
Here in Figure 1 the response time of the OCP system of a
Keysight N7951A 20V, 50A power supply was characterized using the companion
14585A software. It compares response times of 6A and 12A loading when the
current limit is set to 5A. Including the programmed OCP delay time of 5
milliseconds it was found that the actual total response time was 7 milliseconds
for 12A loading and 113 milliseconds for 6A loading.
This is quite different than the response time of an OVP
system. Even if the OCP delay time was set to zero, the response is still on
the order of milliseconds instead of microseconds for the OVP system. And when
the amount of overdrive is small, as is the case for the 6A loading, providing
just 1A of overdrive, the total response time is much greater. Why is that?
Unlike the OVP system, which operates totally independent
of the voltage limit control system, the OCP system is triggered off the
current limit control system. Thus the total response time includes the
response time of the current limit as well. The behavior of a current limit is
quite different than a simple “go/no go” threshold detector as well. A limit system,
or circuit, needs to regulate the power supply’s output at a certain level,
making it a feedback control system. Because of this stability of this system
is important, both with crossing over from constant voltage operation as well
as maintaining a stable output current after crossing over. This leads to the
slower and overdrive dependent response characteristics that are typical of
current limit systems.
So what can be done about the slower response of an OCP
system? Well, early on in this posting I talked about the nature of over
current damage. Generally over current damage is much slower by nature and the
over drive dependent response time is in keeping with time dependent nature of over
current damage. The important thing is understand what the OCP response
characteristic is like and what amount of over current your DUT is able to
sustain, and you should be able to make effective use of the over current
protection capabilities of your system power supply.
Labels:
Advanced Power System,
APS,
constant voltage,
current level,
current limit,
N7900,
OCP,
over voltage protect,
over-current protection,
OVP,
tracking OVP,
Usage
Subscribe to:
Posts (Atom)