Hi everyone,
I am writing this as I am preparing to go to the beach for a week. My topic today will be short but hopefully useful. We are going to talk about a subject that has been near and dear to my heart for the past 15 years, serial versus GPIB communication on our instruments.
Back in the days before LAN and USB became instrument standard interfaces, many of our products were designed with RS-232 serial ports in addition to GPIB. RS-232 is standard on the 681xB AC Source/Analyzers, the E36xxA bench power supplies, the N330xA Electronic loads, as well as a few other products.
RS-232 is an interesting option for communication because it is free, most people have them standard on their computers, and you really only need to buy a reasonably priced cable. The main drawbacks are the fact that you need to put it in remote mode yourself using the "SYST:REM" command, that reasonably priced cable has to be properly configured, and it is slower than GPIB. The main drawbacks of GPIB is that it costs more and you need to purchase hardware.
I did some benchmarking this morning using my trusty 6811B AC Source/Analyzer. I used the proper RS-232 cable and my Keysight 82357B USB to GPIB converter to connect to the 6811B. I wrote a small program that measures the time to send a "*IDN?" command and receive a response. The program looped 100 times and calculated the average time. With GPIB, the average time to send and read back took about 7 ms. With RS-232, the same send command and read back the response took about 50 ms.
So to answer my titular question, "Should I use RS-232 or GPIB to communicate with my instrument?", my answer in every instance would be to use GPIB. I know that it is more expensive but you really get what you pay for in this instance. GPIB is a much faster, more reliable way to communicate with your instruments.
Thanks for reading. Let us know if you have any questions.
Friday, May 29, 2015
Friday, May 22, 2015
New performance options for the N6900A Advance Power System gives greater versatility for your test needs
Our N6900 and N7900 series Advanced Power System (APS) DC
power supplies are some of our most sophisticated products, setting new levels
of performance and capabilities on many fronts. They come in 1kW and 2kW power
levels as shown in Figure 1 and can be grouped together to provide much greater
power levels as needed.
Figure 1: N6900 and N7900 Advanced Power System 1kW and
2kW models
Most noteworthy is that these can be turned into full
two-quadrant DC sources by connecting up the optional 1kW N7909A Power Dissipator
(2 needed for 2kW units) providing 100% power sinking capability. This makes
APS an excellent solution for battery, battery management and many alternative
energy applications, where both sourcing and sinking power are needed.
- The N6900 series DC power supplies are designed for ATE applications where high test throughput and high performance is critical.
- The N7900 series dynamic DC power supplies are designed for ATE applications where high speed dynamic sourcing and measurement is needed, in additions to high performance.
A lot more about these products is covered in another
post on our General Purpose Electronic Test Equipment (GEPTE) blog when they
were first announced. This is a great resource for learning more about APS and
can be accessed from the following link: “New Advanced Power System: Designed to Overcome Your Toughest Test Challenges”
If you are a regular visitor to the “Watt’s Up?” blog no
doubt you have seen we have shared a lot about how to do things with the N6900
series and N7900 series APS to address a number of difficult test challenges. A
lot of times it would have otherwise required additional equipment or custom
hardware to accomplish these tasks. While many of these examples are suitable
for the N6900 and N7900, a good number of times examples make use of the
additional capabilities only available in the N7900 series.
In certain test situations the N6900 series APS would be
a great solution and lower cost than the N7900 series, if only it also had a
certain additional capability. To this end Keysight has recently announced four
new performance options for the N6900 series APS to address a specific test
need you may have, as follows:
- Accuracy Package (option 301): Adds a second seamless measurement range for current
- Measurement Enhancements (Option 302): Adds external data logging and voltage and current digitizers with programmable sample rates
- Source and Speed Enhancements (Option 303): Adds constant dwell arbitrary waveforms and output list capability, and faster up and down programming speed
- Disconnect and Polarity-Reversal Relays (Option 760 and 761): Provides galvanic isolation and allows output voltage to be switched between positive and negative values
Labels:
Advanced Power System,
APS,
Arbs,
LIST,
N6900,
N6900A,
N7900,
N7900A,
output disconnect,
polarity reversal,
seamless measurement ranging,
Selection,
throughput
Wednesday, May 20, 2015
Updates to USB provide higher power and faster charging
For those who regularly visit our blog here are already
aware I do a fair amount of work with regard to test methodologies for
optimizing battery life on mobile wireless devices. One directly related topic
I have been actively investigating these past few months is the battery charging aspects
for these devices. Recharging the battery on these devices takes a considerable
amount of time; typically a couple of hours or longer, and it’s only been
getting worse. However, there has been a lot of work, activity, and even new
product developments that are making dramatic improvements in recharging your
devices’ batteries in less time!
The USB port has become the universal connection for
providing charging power for mobile devices. When initially available a USB
port could provide up to 500 mA for general power for peripheral devices. It
was recognized that this was also a convenient source for charging portable
devices but that more current was needed. The USB BC (battery charging)
standard was established which formalized charging initially for up to 1.5 amps
at 5 volts.
This higher charging current and power was alright for
mobile devices of a couple of generations ago, but today’s smart phones,
tablets, and phablets are using much larger and higher capacity batteries. The end
result is, because USB is 5 volts its power thus limited to 7.5W, that it can
take several hours to recharge a device’s battery. This can be very inconvenient if your battery
goes dead during the day!
Simply increasing the USB current is not a total answer
as this has limitations. First, the micro USB connectors on mobile devices are
rated for no more than about 1.8 to 2 amps. To help on this front there is the
new USB Type-C cable and connector specification released last year. The new type-C
micro connectors are able to handle up to 3 amps and the standard connectors able
to handle up to 5 amps. Higher current alone is not quite enough. Also issued
last year was the new USB Power Delivery 2.0 specification. This specifies a
system capable of providing up to 20 volts and 5 amps. This is more than order
of magnitude improvement in power over the existing USB power. Long charging
times due to power limitations will become a thing of the past.
The new USB power delivery voltages and currents are a
discrete set of levels as shown in table 1. As can be seen the levels depend on
the profile/port designation.
Table 1: USB power delivery 2.0 voltage and current
levels
The cables and connectors of course need to be able to
handle the given level of current and power.
In review of the standard a lot of work and effort has gone into
providing this new capability while maintaining compatibility with the past as
well. Thus for a new mobile device to take advantage of these higher power
levels, it must be capable of negotiating with the charging power port to furnish
it. At the same time, if an earlier generation mobile device is connected, it
will only be able to get the default USB 5 volt level.
I’m looking forward to seeing this new USB power delivery
put into wide-spread use in various innovative new products. Expect to see more
about this topic in future posts from me here!
Labels:
battery charging,
battery life,
battery-powered device,
C rate,
Misc.,
mobile phone,
USB,
USB BC 1.1,
USB Power Delivery 2.0
Thursday, April 30, 2015
When is a number not a number?
All of our power supplies measure their own output voltage and output current. These measured values are available to you from the front panel and over the bus. They may be displayed as an average value or a digitized waveform. Some products have different measurement ranges you can set that affect the accuracy of the measurement and the noise floor of the measurement. Of course, there is a maximum value that each measurement range is capable of measuring. So what happens to the reading if the actual output voltage or current exceeds the maximum value of the measurement range? What does the front panel show and what value do you get if you read it back over the bus?
Below is an example where I set the current measurement range to the 1 mA range on a Keysight N6781A Source/Measure Unit. I then forced more than 1 mA to flow out of the output. As you can see, the front panel indicates “Overload”. If you perform a current measurement and read the result back to your PC, you will get 9.91E37. This is a value defined in the SCPI (Standard Commands for Programmable Instruments) standard to mean “not a number” (NAN). Since Keysight products follow the SCPI standard, we return this number when a range is overloaded. This numeric value for NAN was chosen so that it can be represented as a 32-bit floating point number and is larger than anything expected to occur while using instrumentation. In addition to an overload condition on an instrument, NAN can also be used as the result when, for example, you divide zero by zero or subtract infinity from infinity.
Below is an example where I set the current measurement range to the 1 mA range on a Keysight N6781A Source/Measure Unit. I then forced more than 1 mA to flow out of the output. As you can see, the front panel indicates “Overload”. If you perform a current measurement and read the result back to your PC, you will get 9.91E37. This is a value defined in the SCPI (Standard Commands for Programmable Instruments) standard to mean “not a number” (NAN). Since Keysight products follow the SCPI standard, we return this number when a range is overloaded. This numeric value for NAN was chosen so that it can be represented as a 32-bit floating point number and is larger than anything expected to occur while using instrumentation. In addition to an overload condition on an instrument, NAN can also be used as the result when, for example, you divide zero by zero or subtract infinity from infinity.
This predefined number is also used when waveform data exceeds the maximum rating of a particular range. The screenshot below on the left shows data that does not overload the range. But when the range is changed and part of the waveform exceeds the maximum rating of the range, that part of the waveform data shows up on the screen in red and when returned to a PC, the value is the NAN value of 9.91E37.
Two other unique numbers defined by the SCPI standard are used to represent positive infinity and negative infinity. For positive infinity (INF), 9.9E37 is used. For negative infinity (NINF), -9.9E37 is used. These values can be used to mean “maximum” for a setting. For example, our output voltage slew rate setting has a range of values to which it can be set. If you want to ensure the output voltage will change as quickly as possible, you want to set this to the maximum slew rate possible. Instead of looking up the specification for the maximum setting, you can use the appropriate SCPI command to set the slew rate to 9.9E37 and it will go to the maximum possible slew rate.
So when is a number not a number? When it is equal to 9.91E37!
Labels:
-9.9E37,
9.91E37,
9.9E37,
NAN,
not a number,
overload,
power supply readback,
Usage
Let's See the Watchdog TImer in Action
Hi everybody!
It is the end of the month and time for my monthly blog post.
Quite some time ago, my buddy Gary mentioned our watchdog timer protection in a post. Here is what he had to say:
(For the whole post click here)
Since Gary wrote that post, we have released the N6900 and N7900 APS units that also include this useful feature. What I wanted to do was show how to set it up, how to use it,and how to clear it so that everything is a bit more clear. All of my programming examples in this post will be done using my APS with the VISA-COM IO Library in Visual Basic.
The setup is pretty easy:
APS.WriteString("OUTP:PROT:WDOG:DEL 5")
APS.WriteString("OUTP:PROT:WDOG ON")
This sets the watchdog delay to 5 seconds and enables it. This means that if there is no IO activity (ie your computer hangs up) for 5 seconds, then the unit will go into protect and shut the output down.
Lets say that I have a program that performs a measurement around every second for a minute. Here is the program:
APS.WriteString("OUTP:PROT:WDOG:DEL 2")
APS.WriteString("OUTP:PROT:WDOG ON")
For i = 0 To 59
APS.WriteString("MEAS:VOLT?")
strResponse = APS.ReadString
Threading.Thread.Sleep(1000)
Next
Threading.Thread.Sleep(3000)
APS.WriteString("STAT:QUES:COND?")
strResponse = APS.ReadString
The watchdog delay is set for 2 second so while I run in the loop taking my measurements everything is working great. After the 3 second wait at the end though, the 2 second watchdog timer comes into effect and the unit goes into the protect state and disables the output. The response to the questionsable status query is 2048 which corresponds to bit 11 of the register which is defined as "Output is disabled by a watchdog timer protection". This is the expected result.
My reccomendation to clear the watchdog timer would be to first disable the watchdog timer and then clear the protect. You can then re-start the watchdog timer when you are ready.
APS.WriteString("OUTP:PROT:WDOG OFF")
APS.WriteString("OUTP:PROT:CLE")
The watchdog timer is a pretty cool feature that can perform a pretty useful task. I hope that this blog post explains what it is and how to use it a bit more.
It is the end of the month and time for my monthly blog post.
Quite some time ago, my buddy Gary mentioned our watchdog timer protection in a post. Here is what he had to say:
The watchdog timer is a unique feature on some Agilent power supplies, such as the N6700 series. This feature looks for any interface bus activity (LAN, GPIB, or USB) and if no bus activity is detected by the power supply for a time that you set, the power supply output shuts down. This feature was inspired by one of our customers testing new chip designs. The engineer was running long-term reliability testing including heating and cooling of the chips. These tests would run for weeks or even months. A computer program was used to control the N6700 power supplies that were responsible for heating and cooling the chips. If the program hung up, it was possible to burn up the chips. So the engineer expressed an interest in having the power supply shut down its own outputs if no commands were received by the power supply for a length of time indicating that the program has stopped working properly. The watchdog timer allows you to set delay times from 1 to 3600 seconds.
Since Gary wrote that post, we have released the N6900 and N7900 APS units that also include this useful feature. What I wanted to do was show how to set it up, how to use it,and how to clear it so that everything is a bit more clear. All of my programming examples in this post will be done using my APS with the VISA-COM IO Library in Visual Basic.
The setup is pretty easy:
APS.WriteString("OUTP:PROT:WDOG:DEL 5")
APS.WriteString("OUTP:PROT:WDOG ON")
This sets the watchdog delay to 5 seconds and enables it. This means that if there is no IO activity (ie your computer hangs up) for 5 seconds, then the unit will go into protect and shut the output down.
Lets say that I have a program that performs a measurement around every second for a minute. Here is the program:
APS.WriteString("OUTP:PROT:WDOG:DEL 2")
APS.WriteString("OUTP:PROT:WDOG ON")
For i = 0 To 59
APS.WriteString("MEAS:VOLT?")
strResponse = APS.ReadString
Threading.Thread.Sleep(1000)
Next
Threading.Thread.Sleep(3000)
APS.WriteString("STAT:QUES:COND?")
strResponse = APS.ReadString
The watchdog delay is set for 2 second so while I run in the loop taking my measurements everything is working great. After the 3 second wait at the end though, the 2 second watchdog timer comes into effect and the unit goes into the protect state and disables the output. The response to the questionsable status query is 2048 which corresponds to bit 11 of the register which is defined as "Output is disabled by a watchdog timer protection". This is the expected result.
My reccomendation to clear the watchdog timer would be to first disable the watchdog timer and then clear the protect. You can then re-start the watchdog timer when you are ready.
APS.WriteString("OUTP:PROT:WDOG OFF")
APS.WriteString("OUTP:PROT:CLE")
The watchdog timer is a pretty cool feature that can perform a pretty useful task. I hope that this blog post explains what it is and how to use it a bit more.
Tuesday, April 28, 2015
Optimizing a Power Supply’s Output Response Speed for Applications Demanding Higher Performance
Most basic performance power supplies are intended for
just providing DC power and maintain a stable output for a wide range of load
conditions. They often have lower output bandwidth to achieve this, with the
following consequences:
- Internally this means the feedback loop gain rolls off to zero at a lower frequency, providing relatively greater phase margin. Greater phase margin allows the power supply to remain stable for a wider range of loads, especially larger capacitive loads, when operating as a voltage source.
- Externally this means the output moves slower; both when programming the output to a new voltage setting as well as when recovering from a step change in output load current.
While this is reasonably suited for fairly static DC
powering requirements, greater dynamic output performance is often desirable
for a number of more demanding applications, such as:
- High throughput testing where the power supply’s output needs to change values quickly
- Fast-slewing pulsed current loads where the transient voltage drop needs to be minimized
- Applications where the power supply is used to generate power ARB waveforms
A number of things need to be done to a power supply so
that it will have faster, higher performance output response speed. Primarily
however, this is done by increasing its bandwidth, which means increasing its
loop gain and pushing the loop gain crossover out to a higher frequency. The
consequence of this the power supply’s stability can be more influenced by the
load, especially larger capacitive loads.
To better accommodate a wide range of different loads
many of our higher performance power supplies feature a programmable bandwidth
or programmable output compensation controls. This allows the output to be set
for higher output response speed for a given load, while maintaining stable
operation at the same time. As one example our N7900A series Advanced Power
System (APS) has a programmable output bandwidth control that can be set to Low, for maximum stability, or set to High1, for much greater output voltage response
speed. This can be seen in the graph in Figure 1, taken from the APS user’s
guide.
Figure 1: N7900A APS small signal resistive loading output
voltage response
Low setting
provides maximum stability and so it accommodates a wider range of capacitive
loading. High 1 setting in
comparison is stable for a smaller range of capacitive loading, but allowing
greater response bandwidth. This can be seen in table 1 below, for the
recommended capacitive loading for the N7900A APS, again taken from the APS
user’s guide.
Table 1: N7900A APS recommended maximum capacitive
loading
While a maximum capacitive value is shown for each of the
different APS models for each of the two settings, this is not altogether as
rigid and fixed as it may appear. What is not so obvious is this is based on
the load remaining capacitive over a frequency range roughly comparable to the
power supply’s response bandwidth or beyond. Because of this the capacitor’s
ESR (equivalent series resistance) is an important factor. Beyond the corner
frequency determined by the capacitor’s capacitance and ESR, the capacitor
looks resistive. If this frequency is considerably lower than the power supply’s
response bandwidth, then it has little to no effect on the power supply’s
stability. This is the reason why the power supply is able to charge and
discharge a super capacitor, even though its value is far greater than the capacitance limit given, and not run into stability problems, for example.
One last consideration for more demanding applications
needing fast dynamic output changes, either when changing values or generating ARBs
is the current needed for charging and discharging capacitive loads. Capacitors increasingly become “short-circuits”
to higher AC frequencies, requiring the power supply to be able to drive or
sink very large currents in order to remain effective as a dynamic voltage
source!
.
Labels:
Advanced Power System,
APS,
Arbs,
capacitive loading,
capacitor,
ESR,
loop gain,
N7900A,
output response time,
super capacitor,
transient response,
Usage
Tuesday, March 31, 2015
When is 64,000 points too many?
Hi everybody!
This month's blog post is based off a customer question that we received this month. The question was around arbitrary waveforms (arbs), the number of points for the arb, and waveform fidelity. I have spoken about arbs in the past: click me for Matt's old blog post. Just to quickly reiterate, there are two options for arbs on the N6705 DC Power Analyzer and the N7900 Advanced power System. There is the Constant Dwell (CD) Arb that allows up to 64,000 point with a minimum Dwell time of 10 us per point and there is the standard List Arb that allows up to 512 points with a dwell as low as 1 us per point.
The question that we are trying to answer today is: When is 512 points more than 64,000 points? It is an interesting question to think about. It is definitely not true in cases where you have a non-repeating waveform. The CD Arb will always be the preferred method there and will give you the best fidelity (smallest dwell times).
The answer is when you have long DC levels in your waveform. Let's look at the proposed waveform below (please pardon the picture, I hand drew this on my tablet; also note that it is not to scale):
If you look at this waveform, the total time is 11.5 s. It's a pretty simple waveform that goes from 4 V to 6 V with a 0.05 s ramp between the two values. We need to pay attention to those times.
Lets with the math behind programming a CD Arb. With a CD arb, there is a single dwell time so you basically sample the waveform 64000 times. Lets use that to calculate a dwell time:
11.05 s/64000 = 172.66 us
This means that every point is going to last 172.66 us, no matter if it is in the constantly changing ramp or at a DC level. This means that when the waveform is at 6 V for 10 s, you will use 57,918 points. That is 90% of your points just sitting at 6V! For the 0.05 s ramp, you will only be using 290 points. The ramp is where the waveform is actually changing but due to the nature of how the CD Arb works, you cannot increase the number of points allocated to the ramp.
Let's take a look at the 512 point list now. We know that the first point of the list will be 4 V for 1 s and that the last point of the list will be 6 V for 10 s. That leaves us with 510 points to do the 0.05 s ramp which results in s dwell time of 98 us. This will give us more points in the ramp area and a better looking waveform overall.
That is all I have for this month. Please feel free to use the comments if you'd like to get in touch with us.
This month's blog post is based off a customer question that we received this month. The question was around arbitrary waveforms (arbs), the number of points for the arb, and waveform fidelity. I have spoken about arbs in the past: click me for Matt's old blog post. Just to quickly reiterate, there are two options for arbs on the N6705 DC Power Analyzer and the N7900 Advanced power System. There is the Constant Dwell (CD) Arb that allows up to 64,000 point with a minimum Dwell time of 10 us per point and there is the standard List Arb that allows up to 512 points with a dwell as low as 1 us per point.
The question that we are trying to answer today is: When is 512 points more than 64,000 points? It is an interesting question to think about. It is definitely not true in cases where you have a non-repeating waveform. The CD Arb will always be the preferred method there and will give you the best fidelity (smallest dwell times).
The answer is when you have long DC levels in your waveform. Let's look at the proposed waveform below (please pardon the picture, I hand drew this on my tablet; also note that it is not to scale):
If you look at this waveform, the total time is 11.5 s. It's a pretty simple waveform that goes from 4 V to 6 V with a 0.05 s ramp between the two values. We need to pay attention to those times.
Lets with the math behind programming a CD Arb. With a CD arb, there is a single dwell time so you basically sample the waveform 64000 times. Lets use that to calculate a dwell time:
11.05 s/64000 = 172.66 us
This means that every point is going to last 172.66 us, no matter if it is in the constantly changing ramp or at a DC level. This means that when the waveform is at 6 V for 10 s, you will use 57,918 points. That is 90% of your points just sitting at 6V! For the 0.05 s ramp, you will only be using 290 points. The ramp is where the waveform is actually changing but due to the nature of how the CD Arb works, you cannot increase the number of points allocated to the ramp.
Let's take a look at the 512 point list now. We know that the first point of the list will be 4 V for 1 s and that the last point of the list will be 6 V for 10 s. That leaves us with 510 points to do the 0.05 s ramp which results in s dwell time of 98 us. This will give us more points in the ramp area and a better looking waveform overall.
That is all I have for this month. Please feel free to use the comments if you'd like to get in touch with us.
Subscribe to:
Posts (Atom)