Thursday, June 20, 2013

How can I measure output impedance of a DC power supply?

In my last posting “DC power supply output impedance characteristics”, I explained what the output impedance characteristics of a DC power supply were like for both its constant voltage (CV) and constant current (CC) modes of operation. I also shared an example of what power supply output impedance is useful for. But how does one go about measuring the output impedance of a DC power supply over frequency, if and when needed?

There are a number of different approaches that can be taken, but these days perhaps the most practical is to use a good network analyzer that will operate at low frequencies, ranging from 10 Hz up to 1 MHz, or greater, depending on your needs. Even when using a network analyzer as your starting point there are still quite a few different variations that can be taken.

Measuring the output impedance requires injecting a disturbance at the particular frequency the network analyzer is measuring at. This signal is furnished by the network analyzer but virtually always needs some amount of transformation to be useful. Measuring the output impedance of a voltage source favors driving a current signal disturbance into the output. Conversely, measuring the output impedance of a current source favors driving a voltage signal disturbance into the output. The two set up examples later on here use two different methods for injecting the disturbance.

The reference input “R” of the network analyzer is then used to measure the current while the second input “A” or “T” is used to measure the voltage on the output of the power supply being characterized. Thus the relative gain being measured by the network analyzer is the impedance, based on:
zout = vout/iout = (A or T)/R
The output voltage and current signals need to be compatible with the measurement inputs on the network analyzer. This means a voltage divider probe may be needed for the voltage measurement, depending on the voltage level, and a resistor or current probe will be needed to convert the current into an appropriate voltage signal. A key consideration here is appropriate scaling constants need to be factored in, based on the gain or attenuation of the voltage and current probes being used, so that the impedance reading is correct.



Figure 1: DC power supply output impedance measurement with the Agilent E5061B

One example set up using the Agilent E5061B network analyzer is shown in Figure 1, taken from page 15 of an Agilent E5061B application note on testing DC-DC converters, referenced below. Here the disturbance is injected in through an isolation transformer coupled across the power supply output through a DC blocking capacitor and a 1 ohm resistor. The 1 ohm resistor is doing double duty in that it is changing the voltage disturbance into a current disturbance and it is also providing a means for the “R” input to measure the current. The “T” input then directly measures the DC/DC converter’s (or power supply’s) output voltage.

A second, somewhat more elaborate, variation of this arrangement, based on using a 4395A network analyzer (now discontinued) has been posted by a colleague here on our Agilent Power Supply forum: “Output Impedance Measurement on Agilent Power Supplies”. In this set up the disturbance signal from the network analyzer is instead fed into the analog input of an Agilent N3306A electronic load. The N3306A in turn creates the current disturbance on the output of the DC power supply under test as well as provide any desired DC loading on the power supply’s output. The N3306A can be used to further boost the level of disturbance if needed. Finally, an N278xB active current probe and matching N2779A probe amplifier are used to easily measure the current signal.

Hopefully this will get you on your way if the need for making power supply output impedance ever arises!


Reference: “Evaluating DC-DC Converters and PDN with the E5061B LF-RF Network Analyzer” Application Note, publication number 5990-5902EN (click here to access)

12 comments:

  1. mcafee.com/activate registered trademarks, company names, product names and brand names are the property of their respective owners, and mcafee.com/activate disclaims any ownership in such third-party marks. The use of any third party trademarks, logos, or brand names is for informational purposes only, and does not imply an endorsement by mfmcafee.com or vice versa or that such trademark owner has authorized mfmcafee.com to promote its products or services.

    ReplyDelete

  2. office.com/setup is an independent support and service provider for the most secure remote technical services for all Office products. Our independent support services offer an instant support for all software related errors in the devices, laptops, desktops and peripherals. We have no link or affiliation with any of the brand or third-party company as we independently offer support service for all the product errors you face while using the Office. If your product is under warranty, then you may also avail our support services for free from manufacturer’s official website office.com/setup.

    ReplyDelete
  3. mcafee.com/activate is an independent support and service provider for the most secure remote technical services for all norton products. Our independent support services offer an instant support for all software related errors in the devices, laptops, desktops and peripherals. We have no link or affiliation with any of the brand or third-party company as we independently offer support service for all the product errors you face while using the norton. If your product is under warranty, then you may also avail our support services for free from manufacturer’s official website norton.com/setup.

    ReplyDelete
  4. Thanks for posting this valuable information, really like the way you used to describe. Hope I'll get such posts in future too.

    www.norton.com/setup | www.office.com/setup | www.mcafee.com/activate | www.office.com/setup

    ReplyDelete
  5. Geek Squad Support works effortlessly towards serving the consumers and have a wide stretch toward resolving the issues, our Geek Squad Support provides you with all the answers to your issues.

    ReplyDelete
  6. mcafee.com/activate - Follow the steps to activate mcafee, download and install at www.mcafee.com/activate. Find 25-digit alphanumeric product key on registered email or backside of the retail card to mcafee activate.

    norton.com/setup - Follow the steps to set up Norton, download and install at www.norton.com/setup. Find 25-digit alphanumeric product key on registered email or backside of the retail card to activate norton setup.

    office.com/setup - Enter Key office setup, after purchasing MS Office from visit www.office.com/setup, sign in to your Microsoft account then enter product key for Office Install.

    ReplyDelete
  7. mcafee.com/activate – Facing problems with mcafee products? Get the best instant solution for downloading, installing and activating McAfee Antivirus via mcafee activate and www.mcafee.com/activate.

    norton.com/setup - Learn how to manage, download, install, and activate norton. Visit www.norton.com/setup, Enter norton product key and Install norton setup.

    ReplyDelete
  8. If you still have issue while depositing or withdrawing cryptocurrency from Bittrex, even if you fail to create or login to your Bittrex account, just feel free to get in touch with Bittrex Customer Support services for technical assistance with issues related to Bittrex wallet.

    bittrex support number
    bittrex support phone number
    bittrex support


    You can contact Bittrex tech support representatives via phone call or live chat. They are available 24*7 for the convenience of users.

    bittrex exchange
    bittrex customer service
    bittrex phone number

    ReplyDelete
  9. Step-by-step instructions how to download, install, activate. In case of error uninstall and reinstall your software then contact our Experts.
    office.com/setup
    office setup
    www.office.com/setup

    ReplyDelete
  10. Email customer support number has become an essential contact for every user these days. As a part of our daily lives, whether professional or personal, emailing plays a major role. Even a slight problem can affect the email account. Any loophole in email privacy may risk your data and exchanged email. To understand the importance.Read more about Email customer support number
    email customer service
    sbcglobal customer support
    sbcglobal email support
    email support
    aol email support
    Official ATT Email Help Center where you can find tips and tutorials on using Email and other answers to frequently asked questions.
    att customer services numbers
    att email support
    att email customer service

    ReplyDelete