Today’s system DC power supplies incorporate quite a variety of features to protect both the device under test (DUT) as well as the power supply itself from damage due to a fault condition or setting mishap. Over voltage protect (OVP) and over current protect (OCP) are two core protection features that are found on most all system DC power supplies to help protect against power-related damage.
OVP helps assure the DUT is protected against power-related damage in the event voltage rises above an acceptable range of operation. As over voltage damage is almost instantaneous the OVP level is set at reasonable margin below this level to be effective, yet is suitably higher than maximum expected DUT operating voltage so that any transient voltages do not cause false tripping. Causes of OV conditions are often external to the DUT.
OCP helps assure the DUT is protected against power-related damage in the event it fails in some fashion causing excess current, such as an internal short or some other type of failure. The DUT can also draw excess current from consuming excess power due to overloading or internal problem causing inefficient operation and excessive internal power dissipation.
OVP and OCP are depicted in Figure 1 below for an example DUT that operates at a set voltage level of 48V, within a few percent, and uses about 450W of power. In this case the OVP and OCP levels are set at about 10% higher to safeguard the DUT.
Figure 1: OVP and OCP settings to safeguard an example DUT
However, not all DUTs operate over as limited a range as depicted in Figure 1. Consider for example many, if not most all DC to DC converters operate over a wide range of voltage while using relatively constant power. Similarly many devices incorporate DC to DC converters to give them an extended range of input voltage operation. To illustrate with an example, consider a DC to DC converter that operates from 24 to 48 volts and runs at 225W is shown in Figure 2. DC to DC converters operate very efficiency so they dissipate a small amount of power and the rest is transferred to the load. If there is a problem with the DC to DC converter causing it to run inefficiently it could be quickly damaged due to overheating. While the fixed OCP level depicted here will also adequately protect it for over power at 24 volts, as can be seen it does not work well to protect the DUT for over power at higher voltage levels.
Figure 2: Example DC to DC converter input V and I operating range
A preferable alternative would instead be to have an over power protection limit, as depicted in Figure 3. This would provide an adequate safeguard regardless of input voltage setting.
Figure 3: Example DC to DC converter input V and I operating range with over power protect
As an over power level setting is not a feature that is commonly found in system DC power supplies, this would then mean having to change the OCP level for each voltage setting change, which may not be convenient or desirable, or in some cases practical to do. However, in the Agilent N6900A and N7900A Advance Power System DC power supplies it is possible to continually sense the output power level in the configurable smart triggering system. This can in turn be used to create a logical expression to use the output power level to trigger an output protect shutdown. This is depicted in Figure 4, using the N7906A software utility to graphically configure this logical expression and then download it into the Advance Power System DC power supply. As the smart triggering system operates at hardware speeds within the instrument it is fast-responding, an important consideration for implementing protection mechanisms.
Figure 4: N7906A Software utility graphically configuring an over power protect shutdown
A glitch delay was also added to prevent false triggers due to temporary peaks of power being drawn by the DUT during transient events. While the output power level is being used here to trigger a fault shutdown it could have been just as easily used to trigger a variety of other actions as well.
Monday, June 23, 2014
Safeguarding your power-sensitive DUTs from an over power condition
Labels:
Advanced Power System,
APS,
constant power,
DC/DC converter,
fault protection,
N6900,
N7900,
N7906A,
over power,
over power protect,
over voltage protect,
over-current protection,
OVP,
Usage
Tuesday, June 3, 2014
Upcoming Webinar on High Power Source/Sink Solutions for Testing Bidirectional Energy Devices
Bidirectional and regenerative energy devices both source
and sink power and energy. Correspondingly, a solution that can both source and
sink power and energy is needed for properly testing them. In the past here on
“Watt’s up?” we have talked about what two and four quadrant operation is in our
posting “What is bipolar four quadrant power? (Click here to review). We have
also talked about cross over behavior between sourcing and sinking current with
a DC source that will operate in two quadrants in a two-part posting “Power supply current source-to-sink crossover
characteristics” (Click here to review pt. 1) and (Click here to review pt. 2).
These give useful insights about the nature of multi-quadrant solutions for
bi-directional test applications.
Figure 1: The four operating quadrants
Bidirectional and regenerative energy devices that are
used in many applications, such as satellite power systems, alternative energy,
automotive, and many other areas, operate at kilowatt and higher power levels.
These higher power levels have a significant impact on solutions and approaches
taken to address their testing. Also, the
nature of these bidirectional and regenerative energy devices are not all the
same. This also has an impact in that the capabilities of the test solutions
need to be different to address these different types of devices.
In my upcoming webinar on June 18th, titled “Conquering
the High Power Source/Sink Test Challenge” I will be exploring the test needs
of key bidirectional and regenerative energy devices and then go into the
details of various test solutions and approaches for sourcing and sinking power
and energy, along with their associated advantages and disadvantages. This is
just a couple of weeks away. So if you are involved in this kind of work and are interested, or would just like to learn more, you can register online at the following (click here). In case you cannot join the live event you
will still be able to register and listen to seminar afterward instead, as it
will be recorded. I hope you can join in!
.
Labels:
bipolar,
DC electronic load,
electronic load,
four quadrant,
Misc.,
two quadrant
Friday, May 30, 2014
Arbs! Arbs! Arbs!
Hi everybody,
We have a new intern here and we have recently been talking about the arbitrary waveform capabilities (from now on I will refer to this as arbs) of our power supplies and I thought that this would make an interesting blog post. This is a really cool feature that we offer in our products as it give you the ability to create an alternating signal using our DC power supplies. The two types of arbs are the LIST system and the constant dwell arb.
The LIST arb is a feature that we have in quite a few of our products. The N6700 family, the N7900 family, and even some of our older power supplies have this feature. The "Arb" system in the N6705 DC Power Analyzer is similar to the LIST. These LISTs can contain as many as 512 different points with a timing resolution as low as 1 us. Each point consists of a voltage or current setting and a time. The times can be different for each point. A short example of a programmed LIST is:
VOLT:MODE LIST
LIST:VOLT 10,25,5
LIST:DWEL 5,1,4
In the example above, the voltage will start out at 10 V and stay for 5 seconds, then transition to 25 V for 1 s and then go to 5 V for 4 s. As you can see there are 3 voltage values with 3 corresponding dwell times.
The second mode for arbs that is only available on the N6705B DC Power Analyzer and the N7900 APS is call the Constant Dwell Arb (CD Arb). In this mode, you can program as many as 64K points but all of the defined points have the same dwell time. If we want to do the same waveform as above, we need to choose what will be our dwell time. Since the smallest dwell I used in my example is 1 s, I will choose that. Here is what a small part of the code would look like:
VOLT:MODE ARB
ARB:VOLT:CDW:DWEL 1
ARB:VOLT:CDW 10,10,10,10,10,25,5,5,5,5
The code above will produce the same waveform as the LIST example. CD Arbs can get pretty unwieldy when you have a ton of points but we do offer some tools in our 14585A Control and Analysis software that allow you to import and export csv files to make life a bit easier.
There are advantages and disadvantages to both. As you can see, in some cases it is easier to program a list since it requires less dwell points and gives you more flexibility with what your dwell can be. If your waveform has a lot of DC levels in it, then the standard list might work for you. If you have a long, complex waveform the 64 Kpoints offered in an arb will most likely offer you the best option to replicate your waveform.
Whichever arb you pick, this is a very powerful tool. I am thinking that I will follow this up at a future date with more information about arbs. If you have any questions, feel free to leave us some comments.
We have a new intern here and we have recently been talking about the arbitrary waveform capabilities (from now on I will refer to this as arbs) of our power supplies and I thought that this would make an interesting blog post. This is a really cool feature that we offer in our products as it give you the ability to create an alternating signal using our DC power supplies. The two types of arbs are the LIST system and the constant dwell arb.
The LIST arb is a feature that we have in quite a few of our products. The N6700 family, the N7900 family, and even some of our older power supplies have this feature. The "Arb" system in the N6705 DC Power Analyzer is similar to the LIST. These LISTs can contain as many as 512 different points with a timing resolution as low as 1 us. Each point consists of a voltage or current setting and a time. The times can be different for each point. A short example of a programmed LIST is:
VOLT:MODE LIST
LIST:VOLT 10,25,5
LIST:DWEL 5,1,4
In the example above, the voltage will start out at 10 V and stay for 5 seconds, then transition to 25 V for 1 s and then go to 5 V for 4 s. As you can see there are 3 voltage values with 3 corresponding dwell times.
The second mode for arbs that is only available on the N6705B DC Power Analyzer and the N7900 APS is call the Constant Dwell Arb (CD Arb). In this mode, you can program as many as 64K points but all of the defined points have the same dwell time. If we want to do the same waveform as above, we need to choose what will be our dwell time. Since the smallest dwell I used in my example is 1 s, I will choose that. Here is what a small part of the code would look like:
VOLT:MODE ARB
ARB:VOLT:CDW:DWEL 1
ARB:VOLT:CDW 10,10,10,10,10,25,5,5,5,5
The code above will produce the same waveform as the LIST example. CD Arbs can get pretty unwieldy when you have a ton of points but we do offer some tools in our 14585A Control and Analysis software that allow you to import and export csv files to make life a bit easier.
There are advantages and disadvantages to both. As you can see, in some cases it is easier to program a list since it requires less dwell points and gives you more flexibility with what your dwell can be. If your waveform has a lot of DC levels in it, then the standard list might work for you. If you have a long, complex waveform the 64 Kpoints offered in an arb will most likely offer you the best option to replicate your waveform.
Whichever arb you pick, this is a very powerful tool. I am thinking that I will follow this up at a future date with more information about arbs. If you have any questions, feel free to leave us some comments.
Powerlifting Agilent style!
I have been working out at a gym including lifting weights since the early 1980’s. We have a small gym here in our office building that I use a few times per week. The other day, while doing incline bench presses, my mind was wandering and I began to wonder how much power it took for me to lift the barbell and weights.
I could put the barbell and weights on a battery operated lift we have here in the office and instead of the battery, use one of our power supplies to power the lift and measure the power while operating the lift. I also wanted to calculate how much power would be required. I admit that I had to take out my old physics book to refresh my memory on how to convert weight moved through a distance to watts, but this turned out to be pretty simple: the power is just the force (weight in newtons) times the velocity. Here is the justification:
Force is mass times acceleration. F = mass*acceleration = kg-m/s^2 = newton = N which is weight when the acceleration is due to gravity (weight = mass*gravity).
Work (energy) is force (weight) applied over distance. Work = F*distance = N-m = joule = J.
Power is work per unit of time. Power = J/s = watt = W.
So power in watts = W = J/s = N-m/s = kg-m/s^2-m/s = mass * acceleration * velocity = kg*gravity*velocity = weight*velocity (gravity = 9.8 m/s^2).
During my investigation, I did go off on a tangent for a short time looking at why we talk about measuring weight in kilograms even though kilograms are units for mass and not weight. It would be proper to measure weight in newtons, not in kilograms, but that’s a different story!
So when I lift 205 lbs (93 kg) a distance of 15 inches (0.38 m) in 1.5 seconds, I use 231 watts of power to do so (mass*gravity*velocity = 93 kg * 9.8 m/s^2 * 0.38 m/1.5 s). As I mentioned above, I wanted to see if I could measure something similar with a power supply connected to a battery operated lift by using our power supplies in place of the 24 V batteries. Here is what I found:
I did a baseline power measurement of just the lift lifting some wooden pallets needed to support the barbell I was about to put on the lift. I used 2 Agilent N7972A (40 V, 50 A, 2kW) power supplies connected in parallel (I needed the extra current capacity) and set to 24 V along with our 14585A Control and Analysis Software to capture the power over time. I could then add weight and measure the incremental power required to lift the added weight.
I found that the lift itself consumes 1502 W as my baseline measurement. Then I added a 288 lb (130.6 kg) battery compartment along with 295 lbs (133.8 kg) of barbell weighs for an added 583 lbs (264.4 kg). Again, I measured the power consumed by the lift while it moved the weights vertically and found it to be 1638 W. Lifting the incremental 264.4 kg consumed an additional 136 W. Let’s see if this makes sense with a calculation. The lift moved 4.5 inches vertically in 2.2 seconds which equals 0.052 m/s. The calculated power is then 264.4 kg * 9.8 m/s^2 * 0.052 m/s = 134.7 W. That’s very close to the measured 136 W!!
It is no surprise that the laws of physics work as expected here and that our power supplies can provide insight into those laws. Agilent has added new meaning to the term “powerlifting”!
I could put the barbell and weights on a battery operated lift we have here in the office and instead of the battery, use one of our power supplies to power the lift and measure the power while operating the lift. I also wanted to calculate how much power would be required. I admit that I had to take out my old physics book to refresh my memory on how to convert weight moved through a distance to watts, but this turned out to be pretty simple: the power is just the force (weight in newtons) times the velocity. Here is the justification:
Force is mass times acceleration. F = mass*acceleration = kg-m/s^2 = newton = N which is weight when the acceleration is due to gravity (weight = mass*gravity).
Work (energy) is force (weight) applied over distance. Work = F*distance = N-m = joule = J.
Power is work per unit of time. Power = J/s = watt = W.
So power in watts = W = J/s = N-m/s = kg-m/s^2-m/s = mass * acceleration * velocity = kg*gravity*velocity = weight*velocity (gravity = 9.8 m/s^2).
During my investigation, I did go off on a tangent for a short time looking at why we talk about measuring weight in kilograms even though kilograms are units for mass and not weight. It would be proper to measure weight in newtons, not in kilograms, but that’s a different story!
So when I lift 205 lbs (93 kg) a distance of 15 inches (0.38 m) in 1.5 seconds, I use 231 watts of power to do so (mass*gravity*velocity = 93 kg * 9.8 m/s^2 * 0.38 m/1.5 s). As I mentioned above, I wanted to see if I could measure something similar with a power supply connected to a battery operated lift by using our power supplies in place of the 24 V batteries. Here is what I found:
I did a baseline power measurement of just the lift lifting some wooden pallets needed to support the barbell I was about to put on the lift. I used 2 Agilent N7972A (40 V, 50 A, 2kW) power supplies connected in parallel (I needed the extra current capacity) and set to 24 V along with our 14585A Control and Analysis Software to capture the power over time. I could then add weight and measure the incremental power required to lift the added weight.
I found that the lift itself consumes 1502 W as my baseline measurement. Then I added a 288 lb (130.6 kg) battery compartment along with 295 lbs (133.8 kg) of barbell weighs for an added 583 lbs (264.4 kg). Again, I measured the power consumed by the lift while it moved the weights vertically and found it to be 1638 W. Lifting the incremental 264.4 kg consumed an additional 136 W. Let’s see if this makes sense with a calculation. The lift moved 4.5 inches vertically in 2.2 seconds which equals 0.052 m/s. The calculated power is then 264.4 kg * 9.8 m/s^2 * 0.052 m/s = 134.7 W. That’s very close to the measured 136 W!!
It is no surprise that the laws of physics work as expected here and that our power supplies can provide insight into those laws. Agilent has added new meaning to the term “powerlifting”!
Labels:
N7972A,
power calculation,
power supply,
powerlifting,
Usage
Wednesday, May 21, 2014
DC Source Measurement Accuracy and Resolution – With Shorter Measurement Intervals
I had gotten a customer support request a while ago
inquiring about what the measurement resolution was on our new family of N6900A
and N7900A Advanced Power System (APS) DC sources. Like many of our newer products they utilize
a high-speed digitizing measurement system.
“I cannot find
anything about measurement resolution in the user’s guide, it must have been
overlooked!” I was told. Indeed, we have included the measurement resolution in
the past on our previous products. We did not include it as a single fixed
value this time around, not as an oversight however, but for good reason.
Perhaps the most correct response to the inquiry is “it
depends”. Depends on what? The effective measurement resolution depends on the
measurement interval that is being used. Why is that? Simply put, there is
noise in any measurement system. With older and more basic products that provide
low speed measurements and inherently have a long measurement interval that the
voltage or current signal is integrated over, measurement system noise is
usually not a big factor. However, with the higher speed digitizing measurement
systems we now employ in our performance DC sources, factoring in noise based
on the measurement interval provides a much more realistic and meaningful
answer.
For the N6900A and N7900A APS products we include Table 1
shown below, in our user’s guide to help customers ascertain what the
measurement accuracy and resolution is, based on the measurement interval (i.e.
measurement integration period) being used is.
Table 1: N6900A/N7900A measurement accuracy and resolution
vs. Measurement interval
This table is meant to provide an added error term when
using shorter measurement intervals. We use 1 power line cycle (1 NPLC) as the
reference point at the top of the table, for the measurement accuracy provided
in our specifications. This is a result of averaging 3,255 single samples together.
By doing this we have effectively spread the measurement system noise over a
greater band and filtered it out by the averaging. For voltage measurements the
effective resolution is over 20 bits.
Note now at the bottom of the table there is the row for
one point averaged. It is for 0.003 NPLCs, which is 5 microseconds, the
sampling period of the digitizer in our DC source. For a single sample the
effective measurement resolution is now 12.3 bits for voltage. Note also we
provide an accuracy error adder term of 0.02%. This is taking into account the
measurement repeatability affecting the accuracy.
A convenient expression for converting from number of
bits to dB of signal to noise (SNR) for a digitizer is given by:
SNR (dB) = 6.02 x n (# of bits) + 1.76
The 12.3 bits of effective resolution equates to 75.8 dB of
SNR, which is very much in line with what to expect from a wide band, high
speed digitizing measurement system like what is provided in this product
family.
As previously mentioned the effective measurement
resolution is over 20 bits for a 1 NPLC measurement interval. This actually
happens to be greater than the actual ADC used. While there is less resolution
when using shorter measurement intervals, conversely greater resolution can be
achieved by using longer measurement intervals, which I expect to talk more about
in a future posting here on “Watt’s Up?”!
Wednesday, May 14, 2014
European Space Power Conference (ESPC) for 2014
This week’s blog posting is going in a bit of a different
direction, as I likewise did last month, to attend and participate in the 2014 European
Space Power Conference (ESPC) for 2014. While this was the tenth ESPC, which I
understand takes place every couple of years; this was the first time I had
opportunity to attend. One thing for certain; this was all about DC power,
which is directly aligned with the things I am always involved in. In this particular
instance it was all about DC power for satellites and space-bound crafts and
probes.
I initially found it just a bit curious that a number of
the keynote speeches also focused a fair amount on terrestrial solar power as
well, but I supposed I should not be at all surprised. There has been a large
amount of innovation and a variety of things that benefit our daily lives that
came out of our own space program, fueled by our involvement in the “space
race” and still continuing on to this day. (Can you name a few by chance?).
This is a natural progression for a vast number of technological advances we
enjoy.
At ESPC there were numerous papers presented on solar
cells and arrays, batteries and energy storage, nuclear power sources, power
conversion and DC/DC converters, super-capacitors, and a variety of other
topics related to power. Just a couple of my learnings and observations
include:
·
There was a very high level of collaboration of
sharing findings and answering questions among peers attending the event
·
While batteries generally have very limited
lives, from findings presented, it was interesting to see how well they have
performed over extended periods in space, lasting last well in excess of their
planned life expectancies. It is a reflection of a combination of several
things including careful control and workmanship, understanding life-shortening
and failure mechanisms, how to take properly treat them over time, what should
be expected, as well as other factors contributing to their longevity. I expect
this kind of work will ultimately find its way to being applied to using
lithium ion batteries in automotive as well.
·
A lot of innovation likewise continues with
solar cell development with higher conversion efficiencies coming from
multi-junction devices. Maybe we’ll see this become commonplace for terrestrial
applications before long!
·
A number of research papers were presented from
participants from universities as well. In all, the quality of work was
excellent.
I was there with another colleague, Carlo Canziani. Together
we represented some of our DC power solutions there, including our N7905A DC
Power Analyzer, N7900 series Advanced Power System (APS), and E4360A series Solar
Array Simulator (SAS) mainframe and modules. These are the kinds of advanced
power stimulus and measurement test instruments vital for conducting testing on
satellite and spacecraft power components and systems.
Labels:
Advanced Power System,
DC Power Analyzer,
DC/DC converter,
ESPC,
European Space Power Conference,
Misc.,
N6705B DC Power Analyzer,
N7900,
SAS,
solar array simulator,
solar cell test
Wednesday, April 30, 2014
New Software Update for the N7900 Advanced Power System
Hi everybody,
Last year, we introduced the Agilent N7900 Advanced Power System (hereon in shortened to N7900 APS). The N7900 APS is a full of great features that can only be accessed using the instrument's programming interface. The programming interface works very well but sometimes you just don't want write and troubleshoot a program, you just want something that works.
Well, I have the chance to share some pretty exciting news. We want to provide you software that makes some of these great features easy for you to use. The software is the 14585A Control and Analysis Software. This software was previously only available for the N6705 DC Power Analyzer.
The 14585A software is a standalone application that unlocks three key features: it allows you to look at a graphical representation of the measured data in Scope Mode, create arbitrary waveforms in Arb mode, and log long term data in datalogger mode. These three advanced features can be setup and run by adjusting a few settings and pressing a few buttons.
The software comes with a 30 day free trial so feel free to download it to check it out. Please note that you need at least version A.01.13 of the APS firmware in order to use the software.
You can find the latest APS firmware at:
APS Firmware
You can find the software at:
14585A Software
If you have any questions on the software, feel free to leave us some comments. Thanks for reading!
Last year, we introduced the Agilent N7900 Advanced Power System (hereon in shortened to N7900 APS). The N7900 APS is a full of great features that can only be accessed using the instrument's programming interface. The programming interface works very well but sometimes you just don't want write and troubleshoot a program, you just want something that works.
Well, I have the chance to share some pretty exciting news. We want to provide you software that makes some of these great features easy for you to use. The software is the 14585A Control and Analysis Software. This software was previously only available for the N6705 DC Power Analyzer.
The 14585A software is a standalone application that unlocks three key features: it allows you to look at a graphical representation of the measured data in Scope Mode, create arbitrary waveforms in Arb mode, and log long term data in datalogger mode. These three advanced features can be setup and run by adjusting a few settings and pressing a few buttons.
The software comes with a 30 day free trial so feel free to download it to check it out. Please note that you need at least version A.01.13 of the APS firmware in order to use the software.
You can find the latest APS firmware at:
APS Firmware
You can find the software at:
14585A Software
If you have any questions on the software, feel free to leave us some comments. Thanks for reading!
Subscribe to:
Posts (Atom)