In my last posting “Ferroresonant Transformers as Preregulators
in Early DC Power Supplies “, I introduced the concept of preregulators as a
means of improving the efficiency of power supplies. While a linear regulator provides excellent
performance as a power supply, it has to dissipate all the additional power
resulting from the voltage drop across it as it takes up the difference between
the output voltage setting and the unregulated DC voltage at its input. This
voltage difference becomes quite large for high-line AC input voltage levels,
as well as low DC output voltage settings when the power supply has an
adjustable output. A linear power supply becomes quite inefficient and
physically large, having to dissipate a lot of power in comparison to what it
provides at its output. A preregulator helps
to mitigate this disadvantage while still retaining the performance advantages
of a linear output stage.
The ferroresonant transformer was a clever device and was
an effective means of compensating for variance in the AC input voltage, but
its output was fixed so it did not do anything for compensating for low DC
output voltage settings when the power supply had an adjustable output. A far more common type of preregulator circuit
often used was an SCR preregulator circuit, depicted in Figure 1.
Figure 1: Constant voltage power supply with SCR
preregulator
The SCR is a four layer diode structure. Unlike a conventional
diode it does not conduct in the forward direction until a signal current is
applied to its gate input. It then latches on and remains conducting in its
forward direction. It does so until the forward bias voltage is removed or
reversed and it resets. In the reverse direction it is the same as a
conventional diode. By replacing two of
the conventional diodes in the full wave diode bridge with SCRs as shown in
Figure 1, the DC voltage feeding into the linear regulator output stage can now
be preregulated. The preregulator
control circuit senses the voltage across the series linear regulator output
stage. For each half cycle of the line frequency it adjusts the firing angle of
the SCRs in order to adjust the DC voltage at the input of the linear regulator
so that the voltage across the linear regulator remains constant, compensating
for the load and output voltage level setting accordingly. Figure 2 shows how
changing the firing angle of the SCRs changes the output voltage and current
delivered by the SCR preregulator circuit.
Figure 2: SCR firing angle control of the preregulator’s output
In all, an SCR preregulated power supply with a linear
output stage provided a good balance of efficiency, performance, and cost
making its topology well suited for DC power supplies for a variety of lab and
industrial applications for the time. Still, time marches on and high frequency switching-based
topologies have come to dominate for the most part, due to a number of
advantages they bring. As a matter of fact it is not uncommon today to find a
switching power supply serving as a preregulator as well!